Ensuring the right pressure
Higher demands on throughput and precision – this is only possible with more automation in laboratory technology. Sensapex already equips more than 800 customers worldwide with high-precision micromanipulators, microscopes, and pressure controllers – from neuroscience research to in vitro fertilization (IVF) – to name only a few application examples. To work successfully the pressure controllers from Sensapex rely on the decentralized pressure and vacuum generator PGVA from Festo.
Many experiments in the life sciences depend on highly precise and reliable pressures. In neuroscience research, for example, all steps – from (viral) injection into the intact brain to patch-clamp recordings – require a controlled pressure source. In the past, researchers have even generated pressure by mouth. When higher pressures were required, syringes were used to manually apply pressure through a syringe. But even with gauge readings, neither method produces reproducible results because the stability of pressure application, precise timing and actual pressure levels can vary significantly.
Reproducible results
"We developed the uMc pressure controllers to simplify and automate common tasks in life science experiments while enabling reproducible experiments and workflows," explains Mika Niemi, General Manager of Sensapex, which is part of the Acuvi Group and based in Oulu, northern Finland. Oulu, a city not far away from the Arctic Circle, is known worldwide for its many high-tech companies in electronics and life sciences.
Switching to an automated pressure application allows preset pressure levels to be applied for specific times – either using internal timers or external trigger signals. Modern devices also allow rapid switching between positive and negative pressure. All Sensapex pressure application devices allow the application of externally set pressure levels. This is convenient, for example, to clean a clogged puff micropipette or to briefly increase the pressure before penetrating the connective tissue with a micropipette.
Automated pipette cleaning
Another interesting application for Sensapex pressure controllers is automated pipette cleaning in electrical recordings from single cells. Automated pipette cleaning allows the same patch clamp pipette to be used up to 100 times. During the cleaning process, the uMc micromanipulator moves the pipette to a special cleaning well containing the cleaning agent Tergazyme. The pressure controller generates precise pressure and vacuum, flushing the pipette tip with the cleaning agent. Meanwhile, the user can freely operate other micromanipulators and the microscope during the automatic pipette cleaning process. After cleaning and optional rinsing, the uMp micromanipulator automatically returns the pipette to the starting position and can be used again immediately.
Decentralized pressure and vacuum generator
For Sensapex, an important component for assuring well controlled and reliable application of pressure is the decentralized pressure and vacuum generator PGVA-2 from Festo. PGVA-2 offers a compact complete solution for laboratory applications. It integrates a compressor, air preparation including filtering and buffer storage. Additionally – for the required precise pressure and vacuum control – Sensapex uses up to eight piezo-based proportional pressure regulators VEAB from Festo in their uMc pressure controllers.
“Therefore, Festo’s decentralized PGVA-2 pressure and vacuum generator and the VEAB proportional pressure regulators are exactly the components giving our uMc pressure controllers the precision and reliability they need,” explains Niemi.
In applications, in which built-in regulation is required, the PGVA-1 from Festo is the right choice. This pressure and vacuum generator type integrates the proportional pressure regulators VEAB. The communication relies on a special design web browser based on a graphical user interface (GUI) or a controller. This allows it to operate easily and to have a pressure controller unit in a minimum of space. Regardless of whether laboratory processes such as pipetting medical samples or dispensing with as dosing head are involved, PGVA provides a self-sufficient solution for handling liquids in laboratory applications. All that is needed is a 24-volt power supply to have a pressure- and vacuum-supported solution.
About Acuvi:
Acuvi is a group of companies that provides world-leading systems and technologies that enable higher precision and increased miniaturization. The customers can be found in, among other things, Life Science, the semiconductor industry and advanced optics. Acuvi’s shares are traded on Nasdaq First North Growth Market.
费斯托 (Festo)是一家全球性的独立的家族企业,总部位于德国埃斯林根。自成立以来,Festo在工业自动化技术和技术教育方面制定标准,从而为环境、经济和社会的可持续发展做出贡献。公司为超过35个行业的30万家工厂和过程自动化客户提供气动和电驱动自动化技术解决方案,其中生命科学和实验室自动化业务受到越来越多的关注。Festo产品和服务遍布176个国家。2024年,费斯托在全球61个国家的250多个分支机构拥有约20600名员工,实现销售额34.5亿欧元。每年约8%的销售额用于研发。在这家学习型企业,1.5%的销售额用于基础和进一步培训。Festo 教学培训 (Didactic SE) 是全球领先的技术教育和培训供应商,为全球客户提供工业环境中全面的数字化和常规学习解决方案。