© Festo SE & Co. KG
Air-flow analyser SFGA
Autonomous measuring system with data logger for recording flow rate and pressure directly at the system makes the energy efficiency audit easy.
Torus - image 3
TQ-Lab modular testing station for polymer packaging
Torus image 2
Festo engineers supported by powerful sizing and simulation software created a versatile, modular, and integrated handling solution
Torus image 1
Festo integrated handling solution comes to the fore
© Wellspect
Wellspect - Energy Efficiency Audit
Part of Wellspect's sustainability strategy: Bo Lilja (on the right side), energy efficiency expert at Festo Sweden, conducts the Energy Efficiency Audit in the presence of Erik Blomholt, Maintenance Engineer at Wellspect (on the left side).
© Wellspect
Wellspect - catheter production
Catheter production at Wellspect: By 2025, Wellspect hopes to have reduced the energy consumption for producing each catheter by 12% compared to 2020.
© Festo SE & Co. KG
2023/02/10
|
全球
Saving lives worldwide with low-cost molecular diagnostic tests
Fast MDx shows how many pathogens can be detected with unrivalled speed without the need for expensive ...
阅读新闻稿
Fast MDx shows how many pathogens can be detected with unrivalled speed without the need for expensive biosecure laboratories. This near-patient testing system, developed by London-based company Fast MDx, cuts the typical 24 to 48 hour waiting time to just one to two hours. The new system uses automation technology from Festo.
© Festo SE & Co. KG
Hannes Rößer, Festo
Hannes Rößer, handling technology expert at Festo.