The powerful, compact and versatile HEPP electric gripper is suitable for a wide range of workpieces in electrical systems or applications without compressed air. It is optimized for electronics and small parts production, laboratory automation and special machine construction. 阅读新闻稿 图像 Festo SE & Co. KG 2024/11/07 | 全球 Powerful, compact and precise The powerful, compact and versatile HEPP electric gripper is suitable for a wide range of workpieces ... 阅读新闻稿
Eichenberger successfully held its own against local Chinese manufacturers in the planning of the new Festo gripper due to outstanding quality (5000% more operational performance in the endurance test), production from a single source, years of expertise and close cooperation throughout the development process from start to finish. 阅读新闻稿 图像 Festo SE & Co. KG 2023/11/10 | Global Eichenberger convinces compared to products from ... Eichenberger successfully held its own against local Chinese manufacturers in the planning of the ... 阅读新闻稿
The electric standard gripper EHPS from Festo is the electric version of the pneumatic standard gripper DHPS. The EHPS can be used wherever pneumatics is not permissible. The concept of the electric standard gripper is based on simplicity and low complexity – all the electronics are integrated in the gripper, which means that an external motor controller is not required. 阅读新闻稿 图像 Festo SE & Co. KG 2020/10/01 | 全球 Reliable gripping without air The electric standard gripper EHPS from Festo is the electric version of the pneumatic standard ... 阅读新闻稿