© Festo SE & Co. KG
MolGen - PurePrep TTR
High throughput: the fully automated PurePrep TTR system prepares 320 patient samples per hour for PCR testing. Laboratory-specific automation technology from Festo is included.
Fast MDx 4
Fully automated tests: a separate Festo handling system uses the EHPS-16 electric gripper to transport and position the microwell plate between the individual processing steps.
Fast MDx 3
The automated pipetting system, consisting of the DHOE pipetting head and the DHAO disposable syringe ejector from Festo, can accurately dispense volumes in the range of 10 µl.
Fast MDx 2
High throughput: two Festo 3D gantries with pipetting and transport units ensure a fully automated sequence of molecular diagnostic tests in the Fast MDx.
Fast MDx 1
Richard Lewis, founder and CEO of Fast MDx.
© Festo SE & Co. KG
MolGen - Niels Kruize
Niels Kruize, CEO MolGen
© Wellspect
Wellspect - Energy Efficiency Audit
Part of Wellspect's sustainability strategy: Bo Lilja (on the right side), energy efficiency expert at Festo Sweden, conducts the Energy Efficiency Audit in the presence of Erik Blomholt, Maintenance Engineer at Wellspect (on the left side).
© Wellspect
Wellspect - catheter production
Catheter production at Wellspect: By 2025, Wellspect hopes to have reduced the energy consumption for producing each catheter by 12% compared to 2020.
© Festo SE & Co. KG
2023/02/10
|
Globálně
Saving lives worldwide with low-cost molecular diagnostic tests
Fast MDx shows how many pathogens can be detected with unrivalled speed without the need for expensive ...
Přečíst tiskovou zprávu
Fast MDx shows how many pathogens can be detected with unrivalled speed without the need for expensive biosecure laboratories. This near-patient testing system, developed by London-based company Fast MDx, cuts the typical 24 to 48 hour waiting time to just one to two hours. The new system uses automation technology from Festo.