© Festo SE & Co. KG
2024/09/04
|
アイルランド, イギリス
Festo Controlled Pneumatics
Controlled Pneumatics is the rapidly evolving compressed air technology from Festo that is opening new ...
プレスリリースを閲覧する
Controlled Pneumatics is the rapidly evolving compressed air technology from Festo that is opening new applications for pneumatics. The technology delivers more precision and control than ever, while having the potential to dramatically reduce energy use. This is clearly demonstrated in the VTEP: the first proportional valve terminal on the market, offering high precision, fast response times, and dynamic control.
© Festo SE & Co. KG
Festo SupraMotion 2024: Levitation Gap
The magnetic forces between the superconductor and the carrier on which the containers are transported allow levitation heights of 10 millimeters and more.
© Festo SE & Co. KG
Festo SupraMotion 2024: Filling
Two VTOE dosing heads fill the container with liquid.
© Festo SE & Co. KG
Festo SupraMotion 2024: Decapping
A compact EHMD rotary gripper module opens the screw cap of the container.
© Festo SE & Co. KG
Festo SupraMotion 2024: Entering Clean Room
The contactless levitation module of SupraMotion moves the freeze-dry container into a symbolized clean room.
© Festo SE & Co. KG
Festo SupraMotion 2024
SupraMotion 2024: Opening, closing, filling and weighing in the cleanroom.
© Festo SE & Co. KG
2024/04/23
|
ワールドワイド
Superconductor technology: Contactless working in the laboratory of the future
Superconductor technology enables the contactless movement and handling of objects – ideal for ...
プレスリリースを閲覧する
Superconductor technology enables the contactless movement and handling of objects – ideal for high-tech industries such as laboratory automation or biotechnology. At the Hannover Messe, Festo presents a concept for the fully automated filling and weighing of freeze-dry containers in cleanrooms. Thanks to SupraMotion levitation modules and products from the Festo automation portfolio for laboratory applications, the highest standards of ...
© Festo SE & Co. KG
2024/04/24
|
ワールドワイド
Pneumatics Makes a Technological Leap with Piezo
Controlled Pneumatics is the revolutionary compressed air technology from Festo that is opening up new ...
プレスリリースを閲覧する
Controlled Pneumatics is the revolutionary compressed air technology from Festo that is opening up new perspectives for pneumatics. Thanks to this technology, the pressure control of the compact proportional valve terminal VTEP is extremely sensitive, down to less than 1 mbar. This is perfect for applications such as wafer polishing or patch clamping in life science. In addition, Controlled Pneumatics uses high-precision piezo valves to reduce ...
© Festo SE & Co. KG
2023/11/08
|
ワールドワイド, ドイツ語
A mass flow controller that is silent, fast and cost-effective
 For the gas supply of bioreactors and fermenters or for dosing protective gases - the VEMD mass flow ...
プレスリリースを閲覧する
 For the gas supply of bioreactors and fermenters or for dosing protective gases - the VEMD mass flow controller from Festo delivers maximum control dynamics and costs significantly less than comparable solutions for the control of air, oxygen and inert gases.
© Festo SE & Co. KG
VEMD proportional flow control valve
The proportional flow control valve VEMD is a mass flow controller that is silent, dynamic and affordable, and thus ideal for use in the life sciences, food production or biotechnology.