With the blister packaging machine from IWK, sustainability is not just lip service: with recyclable packaging material, low energy consumption, high speed and ergonomics, the CABLIblue 870 card-to-card blister system is proving to be a real trendsetter. The use of electrical automation technology from Festo increases sustainability and efficiency immensely in this application. Read press release Bild Festo SE & Co. KG 2026/04/24 | Global How packaging machines are becoming more ... With the blister packaging machine from IWK, sustainability is not just lip service: with recyclable ... Read press release
Innovative guide technology, high rigidity and guide load capacity for more load in the same installation space - these are the features of the new ELGD axis family from Festo. In addition, powerful drive elements offer high feed forces and accelerations for shorter cycle times and a long service life. A stainless steel cover strip is friction-free on the outside and does not allow any particles to form there. This makes the drives in the axis family ideal for use in cleanrooms. Read press release Bild Festo SE & Co. KG 2025/12/05 | Global Precise and dynamic Innovative guide technology, high rigidity and guide load capacity for more load in the same ... Read press release
Seeds are the new gold. Why is that? Plant-based foods can feed an ever-growing world population. But climate change, pests and diseases threaten plant breeding. To help develop resistant seeds and make them available to agriculture, plant breeders need vast amounts of DNA. That is precisely why Synchron Lab has developed the "DNA factory", which is automated with handling gantries, electric axes, pneumatic grippers and sensors from Festo. Read press release Bild Festo SE & Co. KG 2023/11/08 | Global Germany A real modular DNA factory Seeds are the new gold. Why is that? Plant-based foods can feed an ever-growing world population ... Read press release
The future belongs to human-robot cooperation. System builder BEC developed such a collaborative solution for Siemens Healthineers. It inserts coils weighing several tonnes precisely into the magnets of magnetic resonance imaging (MRI) machines. Electric cylinders from Festo, which ensure the coils are securely gripped, play a crucial role here. Read press release Bild Festo SE & Co. KG 2022/10/28 | Global Playing it safe in the assembly of MRI machines The future belongs to human-robot cooperation. System builder BEC developed such a collaborative ... Read press release
2024/11/07 | Global SPS 2024 - The Automation Summit in Nuremberg from ... The SPS from 12 – 14 November 2024 in Nuremberg is the industry highlight of the automation sector and, with its large ... Press Releases (7) Images (11) View press kit Bild Festo SE & Co. KG