2023/11/08
ID: 4599

Reliably gripping and turning small parts

The Festo rotary gripper module EHMD in many life science applications

The extremely compact rotary gripper module EHMD is the ideal choice in many life science applications where small objects need to be gripped and turned in confined spaces. For example, it can be used in laboratory automation to open a variety of sample vials with ease. The Z module automatically adjusts to the thread pitches of the caps, eliminating changeover times.

The rotary gripper module EHMD reliably carries out all tasks assigned to it, whether for in vitro diagnostics, cell or genome research or quality inspections in the biotech and pharmaceutical industries. This also applies to preparing and analysing samples, loading centrifuges, gripping, rotating and placing microwell plates or even opening and closing sample vials of different sizes.

 

Combined with a 3D gantry and a camera, it can carry out quality inspections, recognise bar codes, or print labels with a label printer. It is also perfect for use in light assembly or in the electronics industry.

 

Pneumatic or electric

The EHMD comes in a fully electric version or with a pneumatic gripper. Both permit infinite rotation. The optional assembly module with Z compensation automatically adjusts to the thread pitch of the caps without moving the Z-axis. When powered by the Festo motor controller CMMT-ST, it allows sample containers of unknown size to be gripped and turned with variable levels of force.

 

Festo is a global player and an independent family-owned company with headquarters in Esslingen am Neckar, Germany. Festo has set standards in industrial automation technology and technical education ever since its establishment, thereby making a contribution to sustainable development of the environment, the economy and society. The company supplies pneumatic and electrical automation technology to 300,000 customers of factory and process automation in over 35 industries. Digitalization, AI and the LifeTech sector with medical technology and laboratory automation are becoming increasingly important. The products and services are available in 176 countries. With about 20,800 employees in over 250 branch offices in around 60 countries worldwide, Festo achieved a turnover of around €3.81 billion in 2022. Each year around 7% of this turnover is invested in research and development. In this learning company, 1.5 % of turnover is invested in basic and further training. Festo Didactic SE is a leading provider of technical education and training and offers its customers worldwide comprehensive digital and physical learning solutions in the industrial environment.

© Festo SE & Co. KG
Rotary gripper module EHMD
The compact rotary gripper module EHMD comes in a fully electric version or with a pneumatic gripper.