Safety in fail-safe mode
The preconfigured fail-safe circuit in the ready-to-install control cabinet is a safe and low-cost alternative when it comes to fail-safe technology. It replaces a single-acting actuator and guarantees that the actuator assumes a predefined safety position in the event of a pressure and/or power failure.
The fail-safe circuit comes in three different versions, “Fail-Safe Standard“, “Fail-Safe Plus – Always Safe” and “Fail-Safe Plus – Manual Override” to suit different customer requirements. In all three fail-safe versions, the actuator assumes its predefined safety position if the compressed air and/or power supply fails. This is achieved by using compressed air from the reservoir to move the actuator.
This fail-safe circuit, configured by Festo in a ready-to-install control cabinet, is a low-cost and effective safety solution compared with a single-acting linear cylinder. The pre-assembled solutions simplify the engineering process. They are ideal for use in applications such as rainwater overflow tanks in water technology.
Fail-safe times three
If the power and/or compressed air fails, the actuator assumes its predefined safety position. This is the basic functionality provided by the “Fail-Safe Standard” version. With the “Fail-Safe Plus – Always Safe” version, the actuator moves into the predefined safety position unless the circuit is in manual operation. It is possible to switch between manual and automatic operation, but only when compressed air is available.
With the “Fail-Safe Plus – Manual Override” version, the “dominant” manual operation applies. If there is a compressed air and/or power failure, the actuator moves into the predefined safety position unless the circuit is in manual operation. It is possible to switch between manual and automatic operation. In manual operation, the actuator can be moved when there is no compressed air and power until the air reservoir is completely empty. The air reservoir must always be customised in accordance with the customer’s requirements.
Festo es un actor global y una empresa familiar independiente con sede en Esslingen am Neckar (Alemania). Desde sus inicios, Festo ha marcado pautas en la tecnología de automatización industrial y en la formación técnica, contribuyendo así al desarrollo sostenible del medio ambiente, la economía y la sociedad. La empresa suministra tecnología de automatización neumática y eléctrica a 300.000 clientes de automatización de fábricas y procesos en más de 35 sectores. El sector LifeTech, con la tecnología médica y la automatización de laboratorios, es cada vez más importante. Los productos y servicios están disponibles en 176 países de todo el mundo. En todo el mundo, unos 20.600 empleados en cerca de 60 países con más de 250 sucursales generaron unas ventas de aproximadamente 3.450 millones de euros en 2024. De esta cantidad, más del 8% se invierte anualmente en investigación y desarrollo. En la empresa de aprendizaje, las medidas de formación y desarrollo representan el 1,5% de la facturación. Festo Didactic SE es un proveedor líder de educación y formación técnica y ofrece a sus clientes de todo el mundo soluciones integrales de aprendizaje digital y físico en el entorno industrial.