Con la empaquetadora de blísteres de IWK, la sostenibilidad no es sólo palabrería: con material de embalaje reciclable, bajo consumo de energía, alta velocidad y ergonomía, el sistema de blíster tarjeta a tarjeta CABLIblue 870 está demostrando ser un verdadero creador de tendencias. El uso de la tecnología de automatización eléctrica de Festo aumenta enormemente la sostenibilidad y la eficiencia en esta aplicación. Leer nota de prensa Imagen Festo SE & Co. KG 2026/04/24 | Global Cómo las envasadoras son cada vez más sostenibles ... Con la empaquetadora de blísteres de IWK, la sostenibilidad no es sólo palabrería: con material de ... Leer nota de prensa
Hydrogen makes sustainable energy mobile. With the intel ligent trailer control system HY.Runner from GP Joule, transporting hydrogen is more efficient, safer, and more environmentally friendly. The Festo valve terminal VTUG and the solenoid valve VOFC provide a space-saving design on the trailer chassis, as well as additional safety. Leer nota de prensa Imagen Festo SE & Co. KG 2025/10/15 | Global Sustainable, smart, safe Hydrogen makes sustainable energy mobile. With the intel ligent trailer control system HY.Runner ... Leer nota de prensa
Ergonomics improves efficiency thanks to a servo-pneumatic balancer that enables employees in assembly and logistics to lift and move loads effortlessly, using just two fingers. At the heart of the balancer is the powerful and reliable drive solution YHBP from Festo with automatic weight detection and safety Performance Level d – perfect for the automotive and packaging industries. Leer nota de prensa Imagen Festo SE & Co. KG 2024/02/15 | Global Moving loads at the tip of two fingers Ergonomics improves efficiency thanks to a servo-pneumatic balancer that enables employees in ... Leer nota de prensa
The term "sustainability" all too often turns into mere lip service. Not so at Wellspect. This world leader in manufacturing solutions for medical continence care has made sustainability an integral part of its corporate strategy and is committed to putting it into practice. No wonder the company’s plant in Mölndal near Gothenburg, Sweden, relies on Festo Energy Saving Services which save Wellspect €37,000 a year in energy costs. Leer nota de prensa Imagen Wellspect 2023/02/13 | Global €37,000 less energy costs in medical technology The term "sustainability" all too often turns into mere lip service. Not so at Wellspect. This world ... Leer nota de prensa
2024/02/21 | Global Hannover Messe Press Preview 2024 The future of our planet also presents Festo with major challenges. On the one hand, it is about supplying the world's ... Comunicados de prensa (6) Imágenes (20) Ver carpeta de prensa Imagen Festo SE & Co. KG
2023/02/14 | Global Hannover Messe Press Preview 2023 The future of our planet also presents Festo with major challenges. On the one hand, it is about supplying the world's ... Comunicados de prensa (4) Imágenes (23) Ver carpeta de prensa Imagen Festo SE & Co. KG
2022/07/05 | Global 19ª Conferencia de Prensa Internacional de Festo Sostenibilidad en la tecnología de la automatización: ¿algo más que una megatendencia? Las soluciones de automatización ... Comunicados de prensa (5) Imágenes (23) Ver carpeta de prensa Imagen Festo SE & Co. KG