El hecho de que el posicionador funcione en una unidad de control descentralizada, es decir, no directamente en el actuador, abre nuevos horizontes hasta el uso de la inteligencia artificial.
Tableros de mandos en la automatización de procesos
Detectar irregularidades en una etapa temprana e iniciar las medidas necesarias antes de que se produzca un fallo en el sistema se puede hacer ahora con los tableros de mandos de Festo.
Quickly connected to all commonly available fieldbuses: the valve terminal VTUG plug-in, as a new family member of the VG series, is electrically modular and pneumatically flexible - also in the control cabinet.
Electronics manufacturing at the Scharnhausen Technology Plant: Different testing methods ensure high quality. These range from automatic optical inspection (AOI) through in-circuit tests (ICT) to system tests (EOL test).
Electronics manufacturing at the Scharnhausen Technology Plant: Tens of thousands of units of the CPX are assembled according to customer requirements every year. This requires up to 300 different components, including electronic components such...
Integrated drive EMCA: The brushless DC motors from Festo with absolute position recording, integrated regulator, power electronics, absolute encoders.
Integrated drive EMCA: The brushless DC motors from Festo with absolute position recording, integrated regulator, power electronics, absolute encoders.