The extremely compact rotary gripper module EHMD is the ideal choice in many life science applications where small objects need to be gripped and turned in confined spaces. For example, it can be used in laboratory automation to open a variety of sample vials with ease. The Z module automatically adjusts to the thread pitches of the caps, eliminating changeover times. Lire le communiqué de presse Image Festo SE & Co. KG 2023/11/08 | Global Reliably gripping and turning small parts The extremely compact rotary gripper module EHMD is the ideal choice in many life science ... Lire le communiqué de presse
Seeds are the new gold. Why is that? Plant-based foods can feed an ever-growing world population. But climate change, pests and diseases threaten plant breeding. To help develop resistant seeds and make them available to agriculture, plant breeders need vast amounts of DNA. That is precisely why Synchron Lab has developed the "DNA factory", which is automated with handling gantries, electric axes, pneumatic grippers and sensors from Festo. Lire le communiqué de presse Image Festo SE & Co. KG 2023/11/08 | Globale Allemagne A real modular DNA factory Seeds are the new gold. Why is that? Plant-based foods can feed an ever-growing world population ... Lire le communiqué de presse
Saisir des pièces comme la langue d'un caméléon - c'est le principe de fonctionnement de la pince adaptative DHEF de Festo. La pince peut saisir, rassembler et remettre en place des objets de nombreuses formes différentes sans nécessiter de réglage manuel. C'est pourquoi elle a remporté des distinctions renommées en 2020, notamment le iF Design Award et le Red Dot Design Award. Lire le communiqué de presse Image Festo SE & Co. KG 09.04.2020 | Globale La langue de caméléon pour l'automatisation ... Saisir des pièces comme la langue d'un caméléon - c'est le principe de fonctionnement de la pince ... Lire le communiqué de presse