Superconductor technology enables the contactless movement and handling of objects – ideal for high-tech industries such as laboratory automation or biotechnology. At the Hannover Messe, Festo presents a concept for the fully automated filling and weighing of freeze-dry containers in cleanrooms. Thanks to SupraMotion levitation modules and products from the Festo automation portfolio for laboratory applications, the highest standards of cleaning and cleanliness can be met. Lire le communiqué de presse Image Festo SE & Co. KG 2024/04/19 | Globale Superconductor technology: Contactless working in ... Superconductor technology enables the contactless movement and handling of objects – ideal for high ... Lire le communiqué de presse
With the SupraCube, Festo is presenting for the first time a SupraMotion concept in which the superconductor unit can be separated from the electrical cooler and can operate autonomously for up to two hours. The compact technology allows contactless movement and handling of objects - ideal for industries with the highest requirements for cleaning and cleanliness, such as laboratory automation, biotechnology or semiconductor production. Lire le communiqué de presse Image Festo SE & Co. KG 2021/04/12 | Globale SupraCube: Maximum flexibility in automation ... With the SupraCube, Festo is presenting for the first time a SupraMotion concept in which the ... Lire le communiqué de presse
In future-oriented fields such as laboratory automation or biotechnology the requirements placed on the cleaning of production facilities and their purity are very high. With superconductor technology, objects can be moved and handled without contact, which is ideal for such applications. At the Hannover Messe 2020 trade fair, Festo will be presenting the SupraModule concept, which enables wireless control of functions on a magnetic, floating carrier with an autonomous energy supply. Lire le communiqué de presse Image Festo SE & Co. KG 2020/02/12 | Globale SupraModule: Modulare Lösung für die ... In future-oriented fields such as laboratory automation or biotechnology the requirements placed on ... Lire le communiqué de presse
Highly pure, sterile processes are a key challenge for the industrial production – especially in food processing and the pharmaceuticals and medical technology industries, but also in the electronics sector. To keep manufacturing processes as free from contamination as possible, the workpieces and the workroom should be separated from each other. This can be achieved with superconductor-based levitation. Festo will be showing its concept for non-contact weighing and measuring at Achema 2022. Lire le communiqué de presse Image Ruediger J. Vogel 2018/02/12 | Globale Measuring and weighing without contact Highly pure, sterile processes are a key challenge for the industrial production – especially in ... Lire le communiqué de presse