© Festo SE & Co. KG
2024/09/04
|
Irlande, Grande-Bretagne
Festo Controlled Pneumatics
Controlled Pneumatics is the rapidly evolving compressed air technology from Festo that is opening new ...
Lire le communiqué de presse
Controlled Pneumatics is the rapidly evolving compressed air technology from Festo that is opening new applications for pneumatics. The technology delivers more precision and control than ever, while having the potential to dramatically reduce energy use. This is clearly demonstrated in the VTEP: the first proportional valve terminal on the market, offering high precision, fast response times, and dynamic control.
© Festo SE & Co. KG
2024/06/06
|
Globale
Festo Expands its Portfolio with Multilayer Manifolds
Festo is expanding its portfolio to include multilayer manifolds made of plastic (bonded manifolds) in order to ...
Lire le communiqué de presse
Festo is expanding its portfolio to include multilayer manifolds made of plastic (bonded manifolds) in order to be able to offer manufacturers of medical and laboratory equipment solutions from a single source. To this end, Festo is taking over the production systems and processes for manufacturing these complex plastic manifolds from Carville, a leading company in this field.
© Festo SE & Co. KG
Multilayer Manifold
Multilayer manifolds for manufacturers of medical and laboratory equipment: in future, Festo will offer these in combination with media-separated valves from a single source. 
© Festo SE & Co. KG
Festo SupraMotion 2024: Levitation Gap
The magnetic forces between the superconductor and the carrier on which the containers are transported allow levitation heights of 10 millimeters and more.
© Festo SE & Co. KG
Festo SupraMotion 2024: Filling
Two VTOE dosing heads fill the container with liquid.
© Festo SE & Co. KG
Festo SupraMotion 2024: Decapping
A compact EHMD rotary gripper module opens the screw cap of the container.
© Festo SE & Co. KG
Festo SupraMotion 2024: Entering Clean Room
The contactless levitation module of SupraMotion moves the freeze-dry container into a symbolized clean room.
© Festo SE & Co. KG
Festo SupraMotion 2024
SupraMotion 2024: Opening, closing, filling and weighing in the cleanroom.
© Festo SE & Co. KG
Valve block
Valve block with media-separated solenoid valves VYKA from Festo: the high tightness and low energy loss of the valve system increase the efficiency of the machine.