© Festo SE & Co. KG
2024/06/06
|
Globale
Festo Expands its Portfolio with Multilayer Manifolds
Festo is expanding its portfolio to include multilayer manifolds made of plastic (bonded manifolds) in order to ...
Lire le communiqué de presse
Festo is expanding its portfolio to include multilayer manifolds made of plastic (bonded manifolds) in order to be able to offer manufacturers of medical and laboratory equipment solutions from a single source. To this end, Festo is taking over the production systems and processes for manufacturing these complex plastic manifolds from Carville, a leading company in this field.
© Festo SE & Co. KG
Multilayer Manifold
Multilayer manifolds for manufacturers of medical and laboratory equipment: in future, Festo will offer these in combination with media-separated valves from a single source. 
French translation unavailable for Jetzt noch mehr hochwertige elektrische Automatisierungstechnik.
© Festo SE & Co. KG
Festo SupraMotion 2024: Levitation Gap
The magnetic forces between the superconductor and the carrier on which the containers are transported allow levitation heights of 10 millimeters and more.
© Festo SE & Co. KG
Festo SupraMotion 2024: Filling
Two VTOE dosing heads fill the container with liquid.
© Festo SE & Co. KG
Festo SupraMotion 2024: Decapping
A compact EHMD rotary gripper module opens the screw cap of the container.
© Festo SE & Co. KG
Festo SupraMotion 2024: Entering Clean Room
The contactless levitation module of SupraMotion moves the freeze-dry container into a symbolized clean room.
© Festo SE & Co. KG
Festo SupraMotion 2024
SupraMotion 2024: Opening, closing, filling and weighing in the cleanroom.
© Festo SE & Co. KG
2024/04/23
|
Globale
Superconductor technology: Contactless working in the laboratory of the future
Superconductor technology enables the contactless movement and handling of objects – ideal for ...
Lire le communiqué de presse
Superconductor technology enables the contactless movement and handling of objects – ideal for high-tech industries such as laboratory automation or biotechnology. At the Hannover Messe, Festo presents a concept for the fully automated filling and weighing of freeze-dry containers in cleanrooms. Thanks to SupraMotion levitation modules and products from the Festo automation portfolio for laboratory applications, the highest standards of ...
© Festo SE & Co. KG
2024/04/24
|
Globale
Pneumatics Makes a Technological Leap with Piezo
Controlled Pneumatics is the revolutionary compressed air technology from Festo that is opening up new ...
Lire le communiqué de presse
Controlled Pneumatics is the revolutionary compressed air technology from Festo that is opening up new perspectives for pneumatics. Thanks to this technology, the pressure control of the compact proportional valve terminal VTEP is extremely sensitive, down to less than 1 mbar. This is perfect for applications such as wafer polishing or patch clamping in life science. In addition, Controlled Pneumatics uses high-precision piezo valves to reduce ...