© Festo SE & Co. KG
Reconditioning of lithium-ion batteries
System for reconditioning lithium-ion batteries with process automation components such as VZXA angle seat valves, KVZA butterfly valve units, DPFC linear actuators and CPX-MPA valve terminals.
© Festo SE & Co. KG
2024/04/24
|
Globale
Pneumatics Makes a Technological Leap with Piezo
Controlled Pneumatics is the revolutionary compressed air technology from Festo that is opening up new ...
Lire le communiqué de presse
Controlled Pneumatics is the revolutionary compressed air technology from Festo that is opening up new perspectives for pneumatics. Thanks to this technology, the pressure control of the compact proportional valve terminal VTEP is extremely sensitive, down to less than 1 mbar. This is perfect for applications such as wafer polishing or patch clamping in life science. In addition, Controlled Pneumatics uses high-precision piezo valves to reduce ...
© Festo SE & Co. KG
VTEP - use in patch clamping
With the VTEP, it is possible to implement applications such as patch clamping human cells using pressure and vacuum.
© Festo SE & Co. KG
VTEP - use in battery production
The VTEP is suitable for the web control of battery foils, for example.
© Festo SE & Co. KG
VTEP - use in photolithography
Valves such as the VTEP are also used as pilot valves for media valves. In photolithography, for example, a light-resistant layer has to be precisely applied to wafers. A suck-back function ensures that no excess paint escapes.
© Festo SE & Co. KG
Polishing of wafers with VTEP
High-precision control of 5 pressure zones for extremely gentle polishing of wafers with VTEP
© Festo SE & Co. KG
Proportional valve terminal VTEP
Very compact: 10 working channels on an overall width of less than 120 mm
French translation unavailable for Automazione nella produzione di idrogeno verde.
French translation unavailable for Kompakt, modular und kosteneffizient .
© Festo SE & Co. KG
Dr Manuel Loos, Chief Operations Officer ABL GmbH
Dr Manuel Loos, Chief Operations Officer ABL GmbH