© Festo SE & Co. KG
VTEP - use in battery production
The VTEP is suitable for the web control of battery foils, for example.
© Festo SE & Co. KG
VTEP - use in photolithography
Valves such as the VTEP are also used as pilot valves for media valves. In photolithography, for example, a light-resistant layer has to be precisely applied to wafers. A suck-back function ensures that no excess paint escapes.
© Festo SE & Co. KG
Polishing of wafers with VTEP
High-precision control of 5 pressure zones for extremely gentle polishing of wafers with VTEP
© Festo SE & Co. KG
Proportional valve terminal VTEP
Very compact: 10 working channels on an overall width of less than 120 mm
French translation unavailable for Dalla piattaforma CPX-AP-A all'unità valvole VTUG.
© Festo SE & Co. KG
2024/05/07
|
Globale
Many functions safe under the roof of VTUX
Festo is now making it even easier for its users: the functions of the classic valve terminals CPV, MPA-L/S and ...
Lire le communiqué de presse
Festo is now making it even easier for its users: the functions of the classic valve terminals CPV, MPA-L/S and VTUG are now available under the umbrella of the convertible valve terminal VTUX. In addition, the AP-I and AP-A communication system creates the ideal platform for digitalized production. This brings flexibility and openness - true to the motto "Open Architecture".
© Festo SE & Co. KG
VTUX
VTUX: The new valve terminal combines the advantages of three classic valve terminals (photo: Festo)
© Festo SE & Co. KG
2024/05/06
|
Globale
Compact and leak-tight powerhouse
Dosing, aspirating and controlling extremely small quantities of aggressive liquids and gases is not a problem ...
Lire le communiqué de presse
Dosing, aspirating and controlling extremely small quantities of aggressive liquids and gases is not a problem with the media-separated solenoid valve VYKA from Festo. This compact powerhouse has a width of only 7 mm and can dose and aspirate the extremely small amounts of liquid very precisely. It also meets the strict requirements for leak-tightness for gas applications.
© Festo SE & Co. KG
VYKA media-separated solenoid valve
The media-separated solenoid valve VYKA allows the precise dispensing of fluids and the control of liquid flows in manifold duct plates as well as gas flows.
© Festo SE & Co. KG
Sensapex - VEAB proportional pressure regulator from Festo
Sensapex uses up to eight piezo-based proportional pressure regulators VEAB from Festo in their uMc pressure controllers.