© Festo SE & Co. KG
Valves VHEF and VMEF
Manually and mechanically actuated valves VHEF and VMEF from Festo
© Festo SE & Co. KG
2021/04/07
|
Globale
Compact, versatile, powerful
Dosing, aspirating or continuous flow – with the media-separated valves VYKA, VYKB and VZDB from Festo ...
Lire le communiqué de presse
Dosing, aspirating or continuous flow – with the media-separated valves VYKA, VYKB and VZDB from Festo all three operating modes are possible. The compact yet powerful valves dose and aspirate even small quantities with a high level of precision. Thanks to their impressive pressure and nominal width specifications, they are also suitable for controlling the flow in a manifold duct plate, for example.
© Festo SE & Co. KG
Solenoid valves VYKA, VYKB and VZDB
Dosing, aspirating or continuous flow – with the media-separated valves VYKA, VYKB and VZDB from Festo all three operating modes are possible.
© Festo SE & Co. KG
Électrification du groupe motopropulseur, réelle (électromobilité)
La demande d'automatisation pour la production de cellules de batteries et d'autres composants de véhicules électriques est en augmentation. Le degré d'automatisation de la production augmente en raison de l'électrification des...
French translation unavailable for Festo Develops a New Compact Cylinder for its Simplified Electric Motion Series of Actuators .
French translation unavailable for Festo EPCE.
© Festo SE & Co. KG
SupraCube ready for use
Once cooled and disconnected from the cooler, the SupraCube is ready for use: connected in parallel with other SupraCubes on a transport system or for use in the safety lab next door.
© Festo SE & Co. KG
SupraCube: contactless transport
With the SupraCube, objects can be transported without contact - even across covers.
SupraCube
© Festo SE & Co. KG
SupraCube on a transport system
The SupraCube is a Compact stand-alone levitation module with superconductor technology.
SupraCube
© Festo SE & Co. KG
2021/04/12
|
Globale
SupraCube: Maximum flexibility in automation technology
With the SupraCube, Festo is presenting for the first time a SupraMotion concept in which the superconductor ...
Lire le communiqué de presse
With the SupraCube, Festo is presenting for the first time a SupraMotion concept in which the superconductor unit can be separated from the electrical cooler and can operate autonomously for up to two hours. The compact technology allows contactless movement and handling of objects - ideal for industries with the highest requirements for cleaning and cleanliness, such as laboratory automation, biotechnology or semiconductor production.