Face mask - CMMT-ST pic 3
Compatible with higher-level controllers from Beckhoff, Siemens or Rockwell: the CMMT servo drive from Festo.
Face mask_DFM pic 2
Products from Festo’s core range, like the DFM guided drive shown here, enabled the face mask manufacturing system to be built quickly and reliably.
Face mask production system pic 1
Fits in a 20-foot shipping container: Mikron’s system for producing 50-100 protective masks a minute.
VPPI: star of the big screen
The new VPPI proportional pressure regulator from Festo features a large, high definition display that makes set-up and diagnosis a doddle.
© Festo SE & Co. KG
2020/01/23
|
Irlande, Grande-Bretagne
Festo introduces a compact servo drive for demanding positioning applications
Festo has expanded its range of servo drives with the introduction of the CMMT-ST. Complementing the existing ...
Lire le communiqué de presse
Festo has expanded its range of servo drives with the introduction of the CMMT-ST. Complementing the existing CMMT-AS, this new servo drive is equally reliable but much more compact and economical.  These characteristics make it ideal for point-to-point and interpolating motion in demanding applications in assembly and handling technology, packaging machines or in the electronics industry.
© Festo SE & Co. KG
CMMT-ST compact servo drive
The CMMT-ST compact servo drive from Festo offers extremely economical positioning and motion.
© Festo SE & Co. KG
2021/05/24
|
Globale
Precise and robust
The essence of any mechanical switching device is an accurate response. That is exactly why it is designed to ...
Lire le communiqué de presse
The essence of any mechanical switching device is an accurate response. That is exactly why it is designed to respond with precision. And why it can be installed, without backlash, in just a few steps. The manually and mechanically actuated valves from the VHEF and VMEF series from Festo follow precisely these mechanical principles.
© Festo SE & Co. KG
Valve VHEF
The universal, manual stem actuated valve with pushbutton, switch, hand lever or toggle lever attachment.
© Festo SE & Co. KG
Valve VMEF
The universal, mechanical stem actuated valve with roller lever attachment.