© Festo SE & Co. KG
VTOP pneumatic extension modules
Combined to suit the customer’s needs: the pneumatic extension modules of the VTOP with volume booster, failsafe and filter regulator
© Festo SE & Co. KG
2022/01/24
|
Globale
Positioning and SIL: what goes together, grows together
Dosing, mixing, filling – the number of control applications in the process industries is steadily ...
Lire le communiqué de presse
Dosing, mixing, filling – the number of control applications in the process industries is steadily growing and demands high-performance positioners for process valves. Nowadays, extensive diagnostic options such as a pressure-assisted partial stroke test are vital for reliable operation. The new positioner CMSH from Festo for single-acting and double-acting actuators is therefore the perfect highly dynamic, low-wear positioning system for linear ...
© Festo SE & Co. KG
CMSH positioner
The new 2-wire positioner CMSH with HART communication from Festo.
© Festo SE & Co. KG
CMSH positioner on quarter turn actuator with VTOP
Easy and safe installation of the CMSH on the actuator with VTOP with integrated air supply to VDE/VDI 3847-2. This eliminates the need for external piping and significantly reduces the susceptibility to leakages.
French translation unavailable for VPPI – The proportional pressure regulator with the really big display.
French translation unavailable for Virtueller Treff auf echtem Messestand.
2021/03/02
|
Irlande, Grande-Bretagne
Festo introduces the MS2:
The new MS2 air preparation units from industrial automation specialist Festo allows machine builders and ...
Lire le communiqué de presse
The new MS2 air preparation units from industrial automation specialist Festo allows machine builders and design engineers to put precision and accuracy close to the process without compromising on flow rates. The MS2 is designed to deliver the optimum combination of compact design, low weight and high flow rates that are ideally suited to end of arm tooling applications in electronics and small parts assembly.
MS2 air regulator - pic 2
MS2 air regulator - pic 1
Compact, lightweight and with flows up to 350l/min, Festo’s new MS2 air regulators and filters are compact enough to be installed directly on moving components in dynamic applications such as end-of-arm tooling
2020/02/27
|
Irlande, Grande-Bretagne
Festo invests to meet growing demand for electronics components
The semiconductor and electronics industries have set benchmarks for continuous innovation while keeping prices ...
Lire le communiqué de presse
The semiconductor and electronics industries have set benchmarks for continuous innovation while keeping prices low. As digitalisation increases, electronic components are rapidly finding their way into other industries too. Sectors as diverse as the automotive industry, medical technology and distribution logistics are demanding more powerful electronics and sensors for applications ranging from self-driving vehicles to artificial heart valves. ...