© Festo SE & Co. KG
Série de vannes à siège incliné VZXA
Flexible, robuste et performante – la vanne à siège incliné VZXA de Festo régule les débits de fluides de manière rapide et fiable.
© Festo SE & Co. KG
Curing press
Potential savings for loading operations in tire curing presses can now be achieved with the Festo Motion Terminal VTEM.
© Festo SE & Co. KG
Machine de confection de pneus
Un matériau parfait pour la machine de pressage de pneus à chaud : le Motion Terminal  commande désormais les différentes pressions sur la couche de caoutchouc de manière très simple et précise à l'aide d'une application de mouvement.
© Festo SE & Co. KG
AZO CleanDock 3
The pneumatic drives are controlled by the modular, electrical terminal CPX with integrated controller CEC and valve terminal MPA.
© Festo SE & Co. KG
AZO CleanDock 2
The passive section is docked to the active section using pneumatic linear drives from Festo.
© Festo SE & Co. KG
AZO CleanDock 1
The AZO CleanDock – controlled by the automation platform CPX.
© Festo SE & Co. KG
Duerkopp Adler 2
Buttonholes are not only functional but also have a visual aspect. However, in textile manufacturing there is generally very little time to produce them.
© Festo SE & Co. KG
Duerkopp Adler_VUVG
The automatic eyelet buttonholer 581 from Dürkopp Adler delivers the necessary speed. Thanks to the compact Festo solenoid valves VUVG, it takes just under four seconds to create a buttonhole.
© Festo SE & Co. KG
Duerkopp Adler 1
The automatic eyelet buttonholer 581 from Dürkopp Adler delivers the necessary speed. Thanks to the compact Festo solenoid valves VUVG, it takes just under four seconds to create a buttonhole.
© Festo SE & Co. KG
DSBC 2
A fully assembled DSBC cylinder, complete with sensors, fittings and attachments - compiled online with the aid of the Festo Design Tool 3D.