Meeting the CO2 specifications of industrial customers and saving money
Leading industrial companies from the automotive, pharmaceutical and food industries have clear CO2 targets for their products. These require machine builders to make significant energy savings in new machine generations compared with previous machines. This is precisely why Festo offers an unrivalled solution in the global compressed air system market with its energy efficiency module MSE6-C2M.
The energy efficiency module MSE6-C2M from Festo is a global pioneer in monitoring compressed air consumption and supply, automatically detecting leaks as well as the speed of return on investment. This ensures that machines and systems are always available.
Reducing compressed air consumption
When it comes to condition monitoring in compressed air systems, the energy efficiency module not only enables measurement data to be gathered and analysed, but it can also automatically reduce consumption by actively intervening in the supply. Thanks to patented technology from Festo, users can save up to 3.2 metric tons of CO2 and hundreds of euros in operating costs per year, as revealed by calculations and tests.
The energy efficiency module MSE6-C2M combines pressure regulator, on/off valve, sensors and fieldbus communication in one intelligent unit. It monitors the compressed air consumption, shuts off the compressed air after production has stopped for a certain amount of time, and simultaneously prevents the system pressure from falling below a specific stand-by pressure level. This works in a similar way to the automatic stop/start system in a modern car so that no more energy is wasted.
Ready for Industry 4.0
The lower pressure level saves energy, without completely depressurising the system. This means that machines and systems are permanently available. The MSE6-C2M can automatically detect leakages occurring over time and reports these to a controller. It can be fully integrated into the machine network via PROFINET. All measured values such as pressure, flow rate or system parameters are available in the PLC or cloud and can be displayed or individually further processed.
All values in view
Measured values for flow rate, air consumption and pressure can be called up at any time. System operators can use this information as the basis for continuous intelligent energy monitoring of a machine. With the MSE6-C2M it is possible, for example, to determine whether a system is consuming more air now than a year ago, how much compressed air is needed for a production batch, whether the pressure is correctly adjusted or how high the pressure and flow rate were at the time of a machine failure.
Festo est à la fois un acteur mondial et une entreprise familiale indépendante basée à Esslingen am Neckar en Allemagne. Depuis ses débuts, Festo établit des normes en matière de technologie d'automatisation industrielle et de formation technique, contribuant ainsi au développement durable de l'environnement, de l'économie et de la société. La société fournit une technologie d'automatisation pneumatique et électrique à 300 000 clients d'automatisation d'usine et de processus dans plus de 35 industries. Le secteur LifeTech, avec la technologie médicale et l'automatisation des laboratoires, devient de plus en plus important. Les produits et services sont disponibles dans 176 pays du monde. Dans le monde entier, environ 20 800 employés dans environ 60 pays avec plus de 250 succursales ont généré un chiffre d'affaires d'environ 3,81 milliards d'euros en 2022. Sur ce total, environ 7 % sont investis chaque année dans la recherche et le développement. Dans l'entreprise apprenante, les mesures de formation et de développement représentent 1,5 % du chiffre d'affaires. Festo Didactic SE est l'un des principaux fournisseurs d'enseignement et de formation techniques et propose à ses clients du monde entier des solutions complètes d'apprentissage numérique et physique dans l'environnement industriel.