Bij de blisterverpakkingsmachine van IWK is duurzaamheid niet alleen lippendienst: met recyclebaar verpakkingsmateriaal, laag energieverbruik, hoge snelheid en ergonomie bewijst het CABLIblue 870 kaart-naar-kaart blistersysteem een echte trendsetter te zijn. Het gebruik van elektrische automatiseringstechnologie van Festo verhoogt de duurzaamheid en efficiëntie in deze toepassing enorm. Persbericht lezen Afbeelding Festo SE & Co. KG 2026/04/24 | Wereldwijd Hoe verpakkingsmachines duurzamer en efficiënter ... Bij de blisterverpakkingsmachine van IWK is duurzaamheid niet alleen lippendienst: met recyclebaar ... Persbericht lezen
Ergonomics improves efficiency thanks to a servo-pneumatic balancer that enables employees in assembly and logistics to lift and move loads effortlessly, using just two fingers. At the heart of the balancer is the powerful and reliable drive solution YHBP from Festo with automatic weight detection and safety Performance Level d – perfect for the automotive and packaging industries. Persbericht lezen Afbeelding Festo SE & Co. KG 2024/02/15 | Global Moving loads at the tip of two fingers Ergonomics improves efficiency thanks to a servo-pneumatic balancer that enables employees in ... Persbericht lezen
Standardisation is a recipe for success for a fruitful collaboration between packaging machine manufacturers and automation specialists. The strategic partnership between Syntegon and Festo is a great example of this. Thanks to this cooperation, Syntegon was able to simplify its processes and manage the challenges posed by the pandemic and the supply chain crisis more effectively. Persbericht lezen Afbeelding Festo SE & Co. KG 2023/05/03 | Global Standardisation benefits all packaging lines Standardisation is a recipe for success for a fruitful collaboration between packaging machine ... Persbericht lezen
The sustainability of cardboard packaging is leading to its increasing use instead of plastic packaging. A key step in the manufacture of folding boxes is the highly precise gluing of the box blanks. The company Baumer hhs is a specialist and global market leader for applications of this type with its dual-piston pump DPP – supported by the proportional valve VPPM from Festo. Persbericht lezen Afbeelding Festo SE & Co. KG 2023/01/25 | Wereldwijd Ierland Groot-Brittannië Proportional valve technology makes it possible The sustainability of cardboard packaging is leading to its increasing use instead of plastic ... Persbericht lezen
2026/04/24 | Global Interpack 2026 7. tot 13 mei 2026, Messe Düsseldorf Persberichten (7) Afbeeldingen (16) Persmap bekijken Afbeelding Festo SE & Co. KG
2023/05/04 | Global Interpack 2023 International trade fair for the global processing and packaging industry Persberichten (6) Afbeeldingen (24) Persmap bekijken Afbeelding Festo SE & Co. KG