![](https://pressstorageadmin.blob.core.windows.net/prod/styles/content_header/storage-api-public/field/web_images/Configurator32for32process32valve32units321_0.jpg?sv=2017-11-09&sr=b&se=2025-07-24T01:20:07Z&sp=r&sig=6waWQ5kszJoZyBSyhG8sQGy6i45gC19TtfgE2R9LEVo%3D&itok=IYH-eGSN)
Fast and reliable configuration of automated process valves
From manually operated to automated process valves, the new configurator for process valves from Festo makes selecting the optimum solution child's play. Simply select a few parameters and the configurator will immediately suggest appropriate combinations, making engineering in the process industry fast, reliable and easy.
The configurator for process valve units significantly simplifies engineering and procurement processes. The tool ensures quick and successful project management by taking all relevant factors into account: from initial product search, configuration, sizing and documentation right through to ordering and delivery of the ready-to-install process valve unit – including customer-specific requests, everything is combined in one tool.
Configurated process valve units are tailored and ready-to-install, all components are perfectly matched: butterfly valves, quarter turn actuators, pilot valves, sensor boxes, positioners, adapter kits and hand levers. Whatever you are looking for, whether it is the ease of manually actuated combinations, a unit with pilot valves and a sensor box, or a unit with a positioner, you simply choose the required parameters in the input menu and the configurator suggests the right solutions.
Order ID and CAD download included
Together with the proposed solution, the configurator generates an order ID for the complete combination, which can be used for placing future orders. There are also benefits in terms of documentation because the CAD data for the complete module can be downloaded in accordance with the configuration.
Breakthrough in digitalisation
With its configurator for process valve units, Festo is driving digitalisation and supporting its customers to enter the age of Industry 4.0. Festo as an automation expert is combining its extensive knowledge of industrial applications with the latest developments in information technology to realise online applications for industrial automation practice.
Festo is also using digital communication to support its customers throughout the Digital Customer Journey. This digital journey guides users safely and comprehensively through the Festo portfolio, from information procurement and configuration through ordering and delivery to commissioning and maintenance or even to the technical training offering of Festo Didactic.
费斯托 (Festo)是一家全球性的独立的家族企业,总部位于德国埃斯林根。自成立以来,Festo在工业自动化技术和技术教育方面制定标准,从而为环境、经济和社会的可持续发展做出贡献。公司为超过35个行业的30万家工厂和过程自动化客户提供气动和电驱动自动化技术解决方案,其中生命科学和实验室自动化业务受到越来越多的关注。Festo产品和服务遍布176个国家。2023年,费斯托在全球61个国家的250多个分支机构拥有约20600名员工,实现销售额36.5亿欧元。每年约7%的销售额用于研发。在这家学习型企业,1.5%的销售额用于基础和进一步培训。Festo 教学培训 (Didactic SE) 是全球领先的技术教育和培训供应商,为全球客户提供工业环境中全面的数字化和常规学习解决方案。