Festo App wins at the Give a Breath Challenge
On July 29th, Festo and the Fraunhofer IPA were honoured for their developed App "Virus Fighters Handbook" at the Award Ceremony of the Give a Breath Challenge in Munich, an ideas competition organised by Munich Re and the Fraunhofer Society to combat the corona crisis.
In their project, Festo and a team from the Fraunhofer Institute for Manufacturing Engineering and Automation (IPA) joined forces to develop the design of a digital manual based on an existing app in corporation with medical experts from several hospitals. Registered users receive information via the app on the use and maintenance of the newly developed respirators, with specific information provided on treating Covid-19 patients.
With Smartenance, Festo provided an existing and stable platform that only needed minimal reprogramming. The Smartenance software is normally used for the maintenance and servicing of machines and systems in industrial production. The Fraunhofer team, which specialises in the development of didactic material in the field of medical technology, provided the training content.
The Virus Fighters Handbook is to be made available to users worldwide free of charge, as an app for downloading and as a web application.
"I like the entrepreneurial spirit and courage of the team to take the initiative and seize opportunities spontaneously, even outside entrenched structures and processes. Being able to help people around the world fight corona with a purely digital product has given the team a special boost. Festo is proud that their idea has now been awarded a prize", Andreas Oroszi, Head of Digital Business at Festo, says.
Munich Re and the Fraunhofer Gesellschaft launched the Give a Breath Challenge in March. The challenge was split into three categories. The first category was for designs for non-invasive respirator and oxygen concentrators, the second for the development of non-invasive respirator masks, and the third for the provision of information on the use of the equipment developed and basic knowledge on Covid-19 for additional support staff needed. With these three components, a complete respirator system can be set up. It has to be possible to produce the equipment anywhere in the world using 3D printing or other fast manufacturing processes. The primary aim is to create the technological basis for the rapid local supply of respirators to cope with imminent shortages in the local emergency treatment of Covid-19 patients and mitigate the impact of the pandemic for people affected worldwide.
Over 150 project designs from all over the world were submitted to the Challenge. The prize money and the implementation budget for the projects total one million euros.
Video about the Virus Fighters Handbook:
https://youtu.be/D26gtTkhyNk
About Smartenance:
https://getdigitalnow.com/operate/smart-maintenance/smartenance
Landingpage Give a Breath Challenge including press release of Munich Re:
www.munichre.com/giveabreath
#Covid19
#GiveABreathChallenge
费斯托 (Festo)是一家全球性的独立的家族企业,总部位于德国埃斯林根。自成立以来,Festo在工业自动化技术和技术教育方面制定标准,从而为环境、经济和社会的可持续发展做出贡献。公司为超过35个行业的30万家工厂和过程自动化客户提供气动和电驱动自动化技术解决方案,其中生命科学和实验室自动化业务受到越来越多的关注。Festo产品和服务遍布176个国家。2024年,费斯托在全球61个国家的250多个分支机构拥有约20600名员工,实现销售额34.5亿欧元。每年约8%的销售额用于研发。在这家学习型企业,1.5%的销售额用于基础和进一步培训。Festo 教学培训 (Didactic SE) 是全球领先的技术教育和培训供应商,为全球客户提供工业环境中全面的数字化和常规学习解决方案。