How piezo technology more efficiently regulates flow rate and pressure
Precise, energy-saving, silent and fast – for the first time, piezo technology makes gas handling in medical technology and laboratory automation truly efficient. What are the differences compared with proportional solenoid valves? How can specialists in medical technology and laboratory automation easily integrate piezo components into their systems and devices? Festo, the automation specialists, will provide clear answers to these and many more questions in the life science webinar. When? On Wednesday, 6 October 2021 from 3:30 to 4:30 pm CET at the following link: https://www.festo.com/gashandling-webinar
During this webinar engineers and designers in medical technology and laboratory automation, as well as in the production of consumables and disposable products in medicine, diagnostics and laboratories and research facilities will receive a quick overview of the advantages of piezo technology for controlling gases. The participants will get to know the principle and advantages of piezo technology and learn how regulating flow rate and pressure with piezo valves works.
Applications and advantages
Piezo valves use hardly any energy, do not generate heat, are small, light and silent and have a long lifespan. They are approved for air, oxygen and inert gases. Thanks to these properties, they are ideal for mobile, near-patient use in oxygen therapeutic devices or to simulate deceptively real movements in learning robots. But they are also used for dosing shielding gas, for example, when filling infusion bags or for fast surface-mounted laser welding.
During the last fifteen minutes of the webinar, the participants will have the opportunity to ask questions and exchange information with Thomas Kunert, LifeTech Product Manager at Festo. Kunert brings to the table over 30 years of experience in medical technology and 15 years in product management with a focus on piezo technology.
If you cannot attend the live webinar, simply register at the link provided to receive a link to the recording of the webinar.
费斯托 (Festo)是一家全球性的独立的家族企业,总部位于德国埃斯林根。自成立以来,Festo在工业自动化技术和技术教育方面制定标准,从而为环境、经济和社会的可持续发展做出贡献。公司为超过35个行业的30万家工厂和过程自动化客户提供气动和电驱动自动化技术解决方案,其中生命科学和实验室自动化业务受到越来越多的关注。Festo产品和服务遍布176个国家。2024年,费斯托在全球61个国家的250多个分支机构拥有约20600名员工,实现销售额34.5亿欧元。每年约8%的销售额用于研发。在这家学习型企业,1.5%的销售额用于基础和进一步培训。Festo 教学培训 (Didactic SE) 是全球领先的技术教育和培训供应商,为全球客户提供工业环境中全面的数字化和常规学习解决方案。