Precise control of inert gases      
      
        Wherever inert gases need to be precisely controlled, the mass flow controller VEFC from Festo is the right ...      
      阅读新闻稿
     
    
      Wherever inert gases need to be precisely controlled, the mass flow controller VEFC from Festo is the right choice. Thanks to piezo technology, it is compact and flexible, and offers an excellent price/performance ratio. It is especially suitable for use in electronics manufacturing, food production, and anywhere in machine building where shielding gas is required.