Rif010 image 2
De servomotoren van Festo zijn te vinden in de technische ruimte onder de surfpool.
Rif010 image 1
Omdat de golven altijd dezelfde hoogte hebben, zijn de omstandigheden voor surfers ideaal.
© Festo SE & Co. KG
2024/05/07
|
全球, 比利时, 爱尔兰, 荷兰, 英国
Autonomous Flying in a Swarm
For more than 15 years, the Bionic Learning Network has been focusing on the fascination of flying. In addition ...
阅读新闻稿
For more than 15 years, the Bionic Learning Network has been focusing on the fascination of flying. In addition to the technical decoding of bird flight, the team has researched and technologically implemented numerous other flying objects and their natural principles. With the BionicBee, the Bionic Learning Network has now for the first time developed a flying object that can fly in large numbers and completely autonomously in a swarm. The BionicBee ...
© Festo SE & Co. KG
BionicBee - swarm flight
Collision-free flight: To fly in a swarm, the bees follow the paths specified by a central computer.
© Festo SE & Co. KG
BionicBee - Info Graphic
  Functional integration in a small space: The bee’s body contains the compact design for the wing-beating mechanism, the communication technology, and the control components for wing beating and adaptation of the wing geometry.
© Festo SE & Co. KG
BionicBee 2
Natural flight maneuvers with four degrees of freedom: The artificial bee flies with a wingbeat frequency of 15 to 20 hertz. The wings beat forwards and backwards at a 180-degree angle.
© Festo SE & Co. KG
BionicBee 1
The BionicBee is the smallest flying object of the Bionic Learning Network to date. For the first time, the developers used the methodology of generative design.
2024/02/20
|
比利时, 爱尔兰, 荷兰, 英国
Festo electric drive automation at Mondelez
Mondelez has chosen Festo electric drive technology for a new automated chocolate Easter egg mixing ...
阅读新闻稿
Mondelez has chosen Festo electric drive technology for a new automated chocolate Easter egg mixing installation at its site in Herentals, Belgium. The egg mixing line uses an ingenious system of conveyors to ensure that everyone finds a nice mix of flavours in their pack of chocolate eggs at Easter. Electric drives were chosen over pneumatics because they offer lower energy consumption, higher safety and more flexibility in controlling speeds and ...
Mondelez_Image 3
Thanks to Festo electric drives, a variety of flavour mixes can be achieved without difficulty.
Mondelez_Image 2
Dual Festo ELGA timing belt shafts and ESBF electric cylinders direct the filling conveyor in the correct direction to fill the pallet bins evenly.