在Compamed展会上,Festo将通过液体分装应用展示新款CECC-AX控制器。该控制器将PLC编程与Python相结合,从而能够在极小的安装空间内灵活实现各种功能。 因此,该控制器特别适合应用于紧凑型台式设备和子系统中——例如在样本制备、预分析或液体及耗材的自动化处理领域。 阅读新闻稿 图像 Festo SE & Co. KG 2026/10/05 | 全球 适用于生命科学领域灵活应用的紧凑型控制器 在Compamed展会上,Festo将通过液体分装应用展示新款CECC-AX控制器。该控制器将PLC编程与Python相结合,从而能够在极小的安装空间内灵活实现各种功能。 因此 ... 阅读新闻稿
Seeds are the new gold. Why is that? Plant-based foods can feed an ever-growing world population. But climate change, pests and diseases threaten plant breeding. To help develop resistant seeds and make them available to agriculture, plant breeders need vast amounts of DNA. That is precisely why Synchron Lab has developed the "DNA factory", which is automated with handling gantries, electric axes, pneumatic grippers and sensors from Festo. 阅读新闻稿 图像 Festo SE & Co. KG 2023/11/08 | 全球 德国 A real modular DNA factory Seeds are the new gold. Why is that? Plant-based foods can feed an ever-growing world population ... 阅读新闻稿
If there’s one thing the corona pandemic has taught us, it is that laboratories place tremendous importance on high sample throughput rates. Even with highly qualified laboratory personnel, this demand can no longer be met. There’s no getting round the automation of laboratory processes. That’s why MolGen in the Netherlands developed PurePrep TTR, which can prepare 320 patient samples per hour for molecular downstream processing. And the Dutch company uses laboratory-specific automation technology from Festo. 阅读新闻稿 图像 Festo SE & Co. KG 2023/04/24 | 全球 Extremely high sample throughput rates If there’s one thing the corona pandemic has taught us, it is that laboratories place tremendous ... 阅读新闻稿
Dispensing, aspirating, pipetting – precision is a must when handling very small volumes of liquid. So how do specialists in laboratory automation manage to meet their quality requirements reliably and efficiently, even with high throughputs? How do they achieve reproducible results and avoid contamination? The Life Science webinar from automation specialist Festo provides clear answers to these and many other questions. When? On Wednesday, 16 June 2021, from 3:30 to 4:30 pm (CET) at the following link: https://festo.com/liquidhandling-webinar 阅读新闻稿 图像 Festo SE & Co. KG 2021/05/27 | Global How to control precisely very small volumes of ... Dispensing, aspirating, pipetting – precision is a must when handling very small volumes of liquid ... 阅读新闻稿