2020/01/30
ID: 2598

Plug and work with electric drives

Simplified Motion Series from Festo based on digital I/O and IO-Link®

Solving simple motion tasks electrically and intelligent communication from the controller to the cloud via IO-Link® is now possible with the Simplified Motion Series from Festo. The electric drive series combines the simplicity of pneumatics with the benefits of electric automation.

The electric drive series that is part of the Simplified Motion Series is an integrated drive solution for simple motion tasks that enables operation without any software in accordance with the plug and work principle. The parameters for the advancing and retracting speed as well as the pressing and clamping force can be set directly on the drive, along with the reference for the end position, cushioning path and manual operation.

 

Intuitive commissioning

Thanks to the intuitive, quick and easy commissioning directly on the drive, configuration doesn’t require any software or specific know-how. The motion can be simply controlled via digital I/O (DIO), as with a pneumatic valve. End position feedback, which is similar to feedback from a standard proximity sensor, provides information about the completion of the motion task.

 

Advanced user functions are provided via IO-Link®, including convenient remote control, parameter copy, backup function and read functions for advanced process parameters. IO-Link® enables the drives to communicate intelligently from the controllers all the way to the cloud – for simple motions as well as easy handling, commissioning and actuation.

 

Digital I/O and IO-Link® are automatically always on board. This means that products from the Simplified Motion Series contain two types of controllers as standard.

 

Simplified, yet full functionality

Their simplified functionality makes the drives perfect for simple motions between two mechanical end positions, without having to sacrifice optimised motion characteristics, gently cushioned advancing and retracting into the end positions or a simplified pressing and clamping function.

 

At its launch, the Simplified Motion Series will include the following electric drives: spindle and toothed belt axis units ELGS-BS/-TB, mini slide unit EGSS, toothed belt axis unit ELGE-TB, electric cylinder unit EPCS and rotary drive unit ERMS.

Festo is a global player and an independent family-owned company with headquarters in Esslingen am Neckar, Germany. Festo has set standards in industrial automation technology and technical education ever since its establishment, thereby making a contribution to sustainable development of the environment, the economy and society. The company supplies pneumatic and electrical automation technology to 300,000 customers of factory and process automation in over 35 industries. Digitalization, AI and the LifeTech sector with medical technology and laboratory automation are becoming increasingly important. The products and services are available in 176 countries. With about 20,600 employees in over 250 branch offices in around 60 countries worldwide, Festo achieved a turnover of around €3.65 billion in 2023. Each year around 7% of this turnover is invested in research and development. In this learning company, 1.5 % of turnover is invested in basic and further training. Festo Didactic SE is a leading provider of technical education and training and offers its customers worldwide comprehensive digital and physical learning solutions in the industrial environment.

© Festo SE & Co. KG
Simplified Motion Series
The solutions of the Simplified Motion Series from Festo at a glance.
© Festo SE & Co. KG
EPCS
Very economical positioning with the compact electric cylinder EPCS.
© Festo SE & Co. KG
EGSS
Precise and cost-effective positioning with the resilient mini slide EGSS.
© Festo SE & Co. KG
ERMS
Simple and precise swivelling with the heavy-duty rotary drive ERMS.

Global Contact Person

Downloads

Share Press Release