2021/06/30
ID: 3774

Robust and multi-talented

Truly impressive pneumatic drives from the Festo core product range

Pneumatic drives from the Festo core product range have to meet the high demand of offering excellent value for money with the usual high quality for every function. From the compact cylinder ADN-S to the round cylinder DSNU or the mini slide DGST, these drives solve the required motion tasks in the majority of application scenarios, while their sturdiness ensures reliable machines and systems.

Compact cylinder

The compact cylinder ADN-S boasts a housing that is made from one piece and is reduced in weight. In addition to features like sensor markings, a lasered data matrix code and various slots, it is designed to fit perfectly in tight spaces. It is also available in copper-free versions.

 

Round cylinder

Machine designers and fitters will be impressed by the space-saving upgrade of the round cylinder DSNU when it comes to efficient machine design. Its features include several spanner flats as well as injection-moulded polymer bearings. The end-result is a round cylinder to ISO that is even smoother and more user-friendly. Thanks to self-adjusting cushioning PPS, assembly times are significantly reduced. The round cylinder has a Festo Product Key for easy identification and re-ordering.

 

Mini slide

The smallest mini slide on the market now also comes in a version with a symmetrical longitudinal axis. This means that two slides DGST can now sit closely side-by-side to save space, without the compressed air supply having to be installed between them. The mini slide combines precision and power with a high packing density.

Festo is a global player and an independent family-owned company with headquarters in Esslingen am Neckar, Germany. Festo has set standards in industrial automation technology and technical education ever since its establishment, thereby making a contribution to sustainable development of the environment, the economy and society. The company supplies pneumatic and electrical automation technology to 300,000 customers of factory and process automation in over 35 industries. Digitalization, AI and the LifeTech sector with medical technology and laboratory automation are becoming increasingly important. The products and services are available in 176 countries. With about 20,600 employees in over 250 branch offices in around 60 countries worldwide, Festo achieved a turnover of around €3.45 billion in 2024. More than 8% of this turnover is invested in research and development. In this learning company, 1.5 % of turnover is invested in basic and further training. Festo Didactic SE is a leading provider of technical education and training and offers its customers worldwide comprehensive digital and physical learning solutions in the industrial environment.

© Festo SE & Co. KG
ADN-S compact cylinder
Impressive value for money: the compact pneumatic cylinder ADN-S is part of the Festo core product range, which means fast delivery even in large quantities. 
© Festo SE & Co. KG
DSNU round cylinder
Impressive value for money: the round cylinder DSNU is part of the Festo core product range, which means fast delivery even in large quantities. 
© Festo SE & Co. KG
DGST mini slide
Impressive value for money: the mini slide DGST is part of the Festo core product range, which means fast delivery even in large quantities. 

Global Contact Person

Share Press Release