Robust and multi-talented
Pneumatic drives from the Festo core product range have to meet the high demand of offering excellent value for money with the usual high quality for every function. From the compact cylinder ADN-S to the round cylinder DSNU or the mini slide DGST, these drives solve the required motion tasks in the majority of application scenarios, while their sturdiness ensures reliable machines and systems.
Compact cylinder
The compact cylinder ADN-S boasts a housing that is made from one piece and is reduced in weight. In addition to features like sensor markings, a lasered data matrix code and various slots, it is designed to fit perfectly in tight spaces. It is also available in copper-free versions.
Round cylinder
Machine designers and fitters will be impressed by the space-saving upgrade of the round cylinder DSNU when it comes to efficient machine design. Its features include several spanner flats as well as injection-moulded polymer bearings. The end-result is a round cylinder to ISO that is even smoother and more user-friendly. Thanks to self-adjusting cushioning PPS, assembly times are significantly reduced. The round cylinder has a Festo Product Key for easy identification and re-ordering.
Mini slide
The smallest mini slide on the market now also comes in a version with a symmetrical longitudinal axis. This means that two slides DGST can now sit closely side-by-side to save space, without the compressed air supply having to be installed between them. The mini slide combines precision and power with a high packing density.
费斯托 (Festo)是一家全球性的独立的家族企业,总部位于德国埃斯林根。自成立以来,Festo在工业自动化技术和技术教育方面制定标准,从而为环境、经济和社会的可持续发展做出贡献。公司为超过35个行业的30万家工厂和过程自动化客户提供气动和电驱动自动化技术解决方案,其中生命科学和实验室自动化业务受到越来越多的关注。Festo产品和服务遍布176个国家。2024年,费斯托在全球61个国家的250多个分支机构拥有约20600名员工,实现销售额34.5亿欧元。每年约8%的销售额用于研发。在这家学习型企业,1.5%的销售额用于基础和进一步培训。Festo 教学培训 (Didactic SE) 是全球领先的技术教育和培训供应商,为全球客户提供工业环境中全面的数字化和常规学习解决方案。