Space-saving round cylinder with easy adjustment
Impressive time and space savings with the round cylinder DSNU-S-… from Festo. It is the only pneumatic round cylinder with self-adjusting cushioning PPS. This makes commissioning child's play.
The self-adjusting cushioning PPS from Festo puts an end to the back and forth usually required when setting the cushioning of pneumatic cylinders. The cushioning system makes commissioning easier and saves time. This ensures that travel into the end position is dynamic but gentle and doesn't requires any manual intervention.
First save time
Up to now, users had to manually adjust the integrated pneumatic end-position cushioning in the cylinder. This is time-consuming and prolongs the commissioning of systems with lots of drives to be cushioned.
Self-adjusting cushioning PPS from Festo ensures optimum cushioning performance at all times without the need for any manual intervention, even when parameters such as friction and pressure change. This decreases wear and time-consuming impact forces are kept to a minimum.
Then save space
The other benefit of the DSNU-S-… is that it needs less installation space than the round cylinder DSNU from Festo. This is due to its short end cap and smaller mounting thread. It thus supports the trend towards smaller, lighter machines that take up less space, which in turn can have a positive effect on the transport costs.
The DSNU-S-… is part of the Festo core product range, which means short delivery times and worldwide availability. With its attractive price and long service life, the sturdy round cylinder has what it takes to be a bestseller.
Festo is a global player and an independent family-owned company with headquarters in Esslingen am Neckar, Germany. Festo has set standards in industrial automation technology and technical education ever since its establishment, thereby making a contribution to sustainable development of the environment, the economy and society. The company supplies pneumatic and electrical automation technology to 300,000 customers of factory and process automation in over 35 industries. Digitalization, AI and the LifeTech sector with medical technology and laboratory automation are becoming increasingly important. The products and services are available in 176 countries. With about 20,600 employees in over 250 branch offices in around 60 countries worldwide, Festo achieved a turnover of around €3.45 billion in 2024. More than 8% of this turnover is invested in research and development. In this learning company, 1.5 % of turnover is invested in basic and further training. Festo Didactic SE is a leading provider of technical education and training and offers its customers worldwide comprehensive digital and physical learning solutions in the industrial environment.