The twin cylinder DGTZ from Festo is short, flat and extremely versatile. The versatility is ensured by the mounting options on four sides of this rigid and thus non-rotating twin cylinder that is also maintenance-free. Read press release Image Festo SE & Co. KG 2023/03/13 | Global Ideal for tight spaces The twin cylinder DGTZ from Festo is short, flat and extremely versatile. The versatility is ensured ... Read press release
Pneumatic drives from the Festo core product range have to meet the high demand of offering excellent value for money with the usual high quality for every function. From the compact cylinder ADN-S to the round cylinder DSNU or the mini slide DGST, these drives solve the required motion tasks in the majority of application scenarios, while their sturdiness ensures reliable machines and systems. Read press release Image Festo SE & Co. KG 2021/06/30 | Global Robust and multi-talented Pneumatic drives from the Festo core product range have to meet the high demand of offering ... Read press release
Protective masks are in short supply in these times of coronavirus so why not just produce some yourself?! With a system from Mikron, this is almost within everyone’s reach. This scalable system produces 50-100 face masks per minute, depending on the version. With engineering support from Festo, Mikron managed to develop the system in just six weeks. Read press release Image Festo SE & Co. KG 2020/06/10 | Global Mini factories in containers help reduce mask ... Protective masks are in short supply in these times of coronavirus so why not just produce some ... Read press release
Festo designed the new space-saving, flat, DLGF rodless linear drive Read press release Image Festo SE & Co. KG 02/12/2020 | Canada Festo’s DLGF flat design rodless drive fits tight ... Festo designed the new space-saving, flat, DLGF rodless linear drive Read press release