Festo, l'un des leaders mondiaux de la technique d'automatisation, intègre complètement Eichenberger Gewinde AG de Burg en Suisse au 1er avril 2026. À l'avenir, l'entreprise suisse portera le nom de "Festo Gewindetriebe AG". Lire le communiqué de presse Image Festo SE & Co. KG 31.03.2026 | Globale Eichenberger devient Festo Festo, l'un des leaders mondiaux de la technique d'automatisation, intègre complètement Eichenberger ... Lire le communiqué de presse
Controlled Pneumatics is the revolutionary compressed air technology from Festo that is opening up new perspectives for pneumatics. Thanks to this technology, the pressure control of the compact proportional valve terminal VTEP is extremely sensitive, down to less than 1 mbar. This is perfect for applications such as wafer polishing or patch clamping in life science. In addition, Controlled Pneumatics uses high-precision piezo valves to reduce compressed air consumption by up to 50%. Lire le communiqué de presse Image Festo SE & Co. KG 2024/02/05 | Globale Pneumatics Makes a Technological Leap with Piezo Controlled Pneumatics is the revolutionary compressed air technology from Festo that is opening up ... Lire le communiqué de presse
Industrial automation specialist Festo has introduced a new cantilever electro-mechanical drive that is designed to meet the demanding specifications of modern production facilities. The new ELGT drive combines precision with high load-bearing capacity and rigidity, which makes it ideal for small parts and Lithium-ion battery manufacturing. Lire le communiqué de presse Image Festo SE & Co. KG 2022/06/20 | Globale Festo’s new ELGT cantilever electro-mechanical ... Industrial automation specialist Festo has introduced a new cantilever electro-mechanical drive that ... Lire le communiqué de presse
Precisely gluing smartphone displays, applying thermal paste or gluing micro cameras in place are just a selection of the adhesive processes that represent the dosing and dispensing competencies of ViscoTec. Now the company has brought out cartridge applicator units designed for exact and clean feeding of adhesives, pastes and silicones of different viscosities, supported by a pneumatic control module supplied by Festo right to the ViscoTec assembly line as a ready-to-install module. Lire le communiqué de presse Image Festo SE & Co. KG 2021/11/09 | Global High-precision dosing with different viscosities Precisely gluing smartphone displays, applying thermal paste or gluing micro cameras in place are ... Lire le communiqué de presse
13.01.2026 | Globale Grande-Bretagne Productronica 2025 Salon leader mondial pour le développement et la production de l'électronique Communiqués de presse (5) Images (9) Voir le dossier de presse Image Sebastian Resch Photography
2024/11/07 | Global SPS 2024 - The Automation Summit in Nuremberg from ... The SPS from 12 – 14 November 2024 in Nuremberg is the industry highlight of the automation sector and, with its large ... Communiqués de presse (7) Images (11) Voir le dossier de presse Image Festo SE & Co. KG
2023/11/13 | Globale Productronica 2023 World's leading trade fair for electronics development and production where Festo shows latest innovations and solutions ... Communiqués de presse (7) Images (22) Voir le dossier de presse Image Festo SE & Co. KG