© Festo SE & Co. KG
2023/05/15
|
Globale
Dégazage fiable dans la production de cellules de batterie
Le dégazage et l'étanchéité sont des processus essentiels dans la production de ...
Lire le communiqué de presse
Le dégazage et l'étanchéité sont des processus essentiels dans la production de cellules de batterie qui suivent directement le contact initial des cellules de batterie avec une tension électrique. Les cellules de la batterie sont percées de lances et le gaz de formage produit lors de la mise en contact est extrait. Des actionneurs pneumatiques et électriques de Festo sont utilisés pour ...
© Festo SE & Co. KG
Martin Stadler, ViscoTec
Martin Stadler, Managing Director of ViscoTec
© Festo SE & Co. KG
Christian Heidinger, ViscoTec
Christian Heidinger, Head of Product Management at ViscoTec
© Festo SE & Co. KG
2021/11/09
|
Globale
High-precision dosing with different viscosities
Precisely gluing smartphone displays, applying thermal paste or gluing micro cameras in place are just a ...
Lire le communiqué de presse
Precisely gluing smartphone displays, applying thermal paste or gluing micro cameras in place are just a selection of the adhesive processes that represent the dosing and dispensing competencies of ViscoTec. Now the company has brought out cartridge applicator units designed for exact and clean feeding of adhesives, pastes and silicones of different viscosities, supported by a pneumatic control module supplied by Festo right to the ViscoTec assembly ...
© Festo SE & Co. KG
ViscoTec eco-FEED
The latest devices for automatically and evenly emptying double-chamber cartridges are called eco-FEED (shown here) and vipro-FEED DC. The control module is integrated in the lower section. The cartridge applicator cylinders as well as the double...
© Festo SE & Co. KG
Control module for ViscoTec
The heart of the system: the control module supplied ready for installation by Festo monitors the pressure and quality of the adhesive application independently of temperature and viscosity.
2021/10/20
|
Irlande, Grande-Bretagne
Grolsch bottling plant upgrade goes with a swing, thanks to Festo automation
New servo technology from Festo is helping Grolsch to put the iconic swing tops on its bottles of lager. The ...
Lire le communiqué de presse
New servo technology from Festo is helping Grolsch to put the iconic swing tops on its bottles of lager. The ‘swing-top transfer unit’ was custom-designed by Festo in conjunction with system integrator MCA Linear Motion Robotics and is installed at the Grolsch Enschede plant in The Netherlands.
© Festo SE & Co. KG
Grolsch pic 2
The Grolsch 'swing-top transfer unit' features the new Festo EMMT servo motor and CPX-E automation system and provides approximately 3,800 bottles per hour with a porcelain cap and rubber ring.
Grolsch pic 1
New servo technology from Festo is helping Grolsch to put the iconic swing tops on its bottles of lager.
© Festo SE & Co. KG
ViscoTec – applying of thermal paste
Maximum dispensing precision with systems from market leader ViscoTec, whether gluing smartphone displays and mini cameras or applying thermal paste.