2024/02/20
|
Belgique, Irlande, Pays-Bas, Grande-Bretagne
Festo electric drive automation at Mondelez
Mondelez has chosen Festo electric drive technology for a new automated chocolate Easter egg mixing ...
Lire le communiqué de presse
Mondelez has chosen Festo electric drive technology for a new automated chocolate Easter egg mixing installation at its site in Herentals, Belgium. The egg mixing line uses an ingenious system of conveyors to ensure that everyone finds a nice mix of flavours in their pack of chocolate eggs at Easter. Electric drives were chosen over pneumatics because they offer lower energy consumption, higher safety and more flexibility in controlling speeds and ...
Mondelez_Image 3
Thanks to Festo electric drives, a variety of flavour mixes can be achieved without difficulty.
Mondelez_Image 2
Dual Festo ELGA timing belt shafts and ESBF electric cylinders direct the filling conveyor in the correct direction to fill the pallet bins evenly.
Mondelez_Image 1
Bob Aerts (Engineering Mondelez) together with Johan De Pauw (Sales Engineer from Festo) at the new filling system.
© Festo SE & Co. KG
2024/02/15
|
Globale
Moving loads at the tip of two fingers
Ergonomics improves efficiency thanks to a servo-pneumatic balancer that enables employees in assembly and ...
Lire le communiqué de presse
Ergonomics improves efficiency thanks to a servo-pneumatic balancer that enables employees in assembly and logistics to lift and move loads effortlessly, using just two fingers. At the heart of the balancer is the powerful and reliable drive solution YHBP from Festo with automatic weight detection and safety Performance Level d – perfect for the automotive and packaging industries.
© Festo SE & Co. KG
2024/04/24
|
Globale
Pneumatics Makes a Technological Leap with Piezo
Controlled Pneumatics is the revolutionary compressed air technology from Festo that is opening up new ...
Lire le communiqué de presse
Controlled Pneumatics is the revolutionary compressed air technology from Festo that is opening up new perspectives for pneumatics. Thanks to this technology, the pressure control of the compact proportional valve terminal VTEP is extremely sensitive, down to less than 1 mbar. This is perfect for applications such as wafer polishing or patch clamping in life science. In addition, Controlled Pneumatics uses high-precision piezo valves to reduce ...
© Festo SE & Co. KG
VTEP - use in patch clamping
With the VTEP, it is possible to implement applications such as patch clamping human cells using pressure and vacuum.
© Festo SE & Co. KG
VTEP - use in battery production
The VTEP is suitable for the web control of battery foils, for example.
© Festo SE & Co. KG
VTEP - use in photolithography
Valves such as the VTEP are also used as pilot valves for media valves. In photolithography, for example, a light-resistant layer has to be precisely applied to wafers. A suck-back function ensures that no excess paint escapes.