© Festo SE & Co. KG
Polishing of wafers with VTEP
High-precision control of 5 pressure zones for extremely gentle polishing of wafers with VTEP
© Festo SE & Co. KG
Proportional valve terminal VTEP
Very compact: 10 working channels on an overall width of less than 120 mm
French translation unavailable for Dalla piattaforma CPX-AP-A all'unità valvole VTUG.
French translation unavailable for Produzione sicura di idrogeno mediante elettrolisi.
French translation unavailable for Idrogeno verde per diversi settori industriali.
French translation unavailable for Immagazzinare l'idrogeno verde.
French translation unavailable for Automazione nella produzione di idrogeno verde.
© Festo SE & Co. KG
2024/01/17
|
Globale
80% more productivity in 3D printing
"Our aim is to achieve a high level of maturity of CNC machines with our additive manufacturing ...
Lire le communiqué de presse
"Our aim is to achieve a high level of maturity of CNC machines with our additive manufacturing machines," explains Dr. Vino Suntharakumaran, Managing Director at DMG MORI Additive GmbH. The company is not far off reaching this aim with the LASERTEC 30 DUAL SLM, which increases productivity by 80%. Festo has been brought on board as a development partner. Thanks to its ready-to-install automation solution, the inert gas atmosphere is ...
© Festo SE & Co. KG
DMG MORI Additive - ready-to-install complete solution
Safe inert gas atmosphere for stable processes in additive manufacturing thanks to a ready-to-install complete solution from Festo.
© Festo SE & Co. KG
DMG MORI Additive - Dr. Vino Suntharakumaran
Dr. Vino Suntharakumaran, Managing Director at DMG MORI Additive GmbH