© Festo SE & Co. KG
2024/05/06
|
ワールドワイド
Automated nitrogen analysis reduces costs per sample
The world's population is growing and with it the demand for food and animal feed with clearly verifiable ...
プレスリリースを閲覧する
The world's population is growing and with it the demand for food and animal feed with clearly verifiable ingredients. This includes the protein content. This can be determined by nitrogen analysis – fully automaticated with the new N-Realyzer from C. Gerhardt. The laboratory system ensures high throughput, is low-maintenance and intuitive to operate. Among other things, it owes this to a valve block from Festo, which offers high tightness in ...
© Festo SE & Co. KG
Nils Müller, C. Gerhardt
Nils Müller, Head of Research and Development at C. Gerhardt
© Festo SE & Co. KG
N-Realyzer
Automated nitrogen analysis to determine protein content: the N-Realyzer from C. Gerhardt increases productivity and significantly reduces costs per sample. .
© Festo SE & Co. KG
2024/04/24
|
ワールドワイド
Pneumatics Makes a Technological Leap with Piezo
Controlled Pneumatics is the revolutionary compressed air technology from Festo that is opening up new ...
プレスリリースを閲覧する
Controlled Pneumatics is the revolutionary compressed air technology from Festo that is opening up new perspectives for pneumatics. Thanks to this technology, the pressure control of the compact proportional valve terminal VTEP is extremely sensitive, down to less than 1 mbar. This is perfect for applications such as wafer polishing or patch clamping in life science. In addition, Controlled Pneumatics uses high-precision piezo valves to reduce ...
© Festo SE & Co. KG
VTEP - use in patch clamping
With the VTEP, it is possible to implement applications such as patch clamping human cells using pressure and vacuum.
© Festo SE & Co. KG
2023/11/08
|
ワールドワイド, ドイツ語
A mass flow controller that is silent, fast and cost-effective
 For the gas supply of bioreactors and fermenters or for dosing protective gases - the VEMD mass flow ...
プレスリリースを閲覧する
 For the gas supply of bioreactors and fermenters or for dosing protective gases - the VEMD mass flow controller from Festo delivers maximum control dynamics and costs significantly less than comparable solutions for the control of air, oxygen and inert gases.
© Festo SE & Co. KG
VEMD proportional flow control valve
The proportional flow control valve VEMD is a mass flow controller that is silent, dynamic and affordable, and thus ideal for use in the life sciences, food production or biotechnology.
© Festo SE & Co. KG
EHMD in laboratory automation
The compact rotary gripper module EHMD from Festo can handle virtually any gripping task in laboratory automation, no matter how small.  
© Festo SE & Co. KG
2024/05/02
|
ワールドワイド
Reliably gripping and turning small parts
The extremely compact rotary gripper module EHMD is the ideal choice in many life science applications where ...
プレスリリースを閲覧する
The extremely compact rotary gripper module EHMD is the ideal choice in many life science applications where small objects need to be gripped and turned in confined spaces. For example, it can be used in laboratory automation to open a variety of sample vials with ease. The Z module automatically adjusts to the thread pitches of the caps, eliminating changeover times.