© Festo SE & Co. KG
MolGen - Pipetting
Extremely small pipetting volumes: the second robot arm with the pipetting head distributes liquids onto a microwell plate.
© Festo SE & Co. KG
MolGen - Opening vial
During the initial work operation, the first robot arm grasps a sample vial by the cap with an electric gripper and brings it into a position at which the cap is removed.
© Festo SE & Co. KG
MolGen - Gripping vial
During the initial work operation, the first robot arm grasps a sample vial by the cap with an electric gripper and brings it into a position at which the cap is removed.
© Festo SE & Co. KG
MolGen - PurePrep TTR
High throughput: the fully automated PurePrep TTR system prepares 320 patient samples per hour for PCR testing. Laboratory-specific automation technology from Festo is included.
Japanese translation unavailable for Festo Breaks Price/Performance Barriers with New Multi-Axis Gantry .
Japanese translation unavailable for Festo Advances High-Throughput Automated Pipetting with Closed-Loop Control.
Japanese translation unavailable for EXCL gantry top view.
Japanese translation unavailable for Closed-loop pipette head.
© Festo SE & Co. KG
2023/02/10
|
ワールドワイド
Saving lives worldwide with low-cost molecular diagnostic tests
Fast MDx shows how many pathogens can be detected with unrivalled speed without the need for expensive ...
プレスリリースを閲覧する
Fast MDx shows how many pathogens can be detected with unrivalled speed without the need for expensive biosecure laboratories. This near-patient testing system, developed by London-based company Fast MDx, cuts the typical 24 to 48 hour waiting time to just one to two hours. The new system uses automation technology from Festo.