© Festo SE & Co. KG
Synchron - modular DNA factory
With this system 40,000 DNA samples from plants can be extracted fully automatically per day.
© Sens
2023/11/08
|
ワールドワイド, ドイツ語
Ensuring the right pressure
Higher demands on throughput and precision – this is only possible with more automation in laboratory ...
プレスリリースを閲覧する
Higher demands on throughput and precision – this is only possible with more automation in laboratory technology. Sensapex already equips more than 800 customers worldwide with high-precision micromanipulators, microscopes, and pressure controllers – from neuroscience research to in vitro fertilization (IVF) – to name only a few application examples. To work successfully the pressure controllers from Sensapex rely on the decentralized ...
© Festo SE & Co. KG
Sensapex - PGVA-2 pressure and vacuum generator from Festo
For Sensapex, an important component for delivering well controlled and reliable application of pressure is the decentralized pressure and vacuum generator PGVA-2 from Festo.
© Festo SE & Co. KG
Sensapex - VEAB proportional pressure regulator from Festo
Sensapex uses up to eight piezo-based proportional pressure regulators VEAB from Festo in their uMc pressure controllers.
© Sensapex
Sensapex - Mika Niemi
Mika Niemi, General Manager of Sensapex
© Sens
Sensapex - complete system
A complete solution for higher throughput and accuracy in lab automation – including microscopes and pressure controllers from Sensapex as well as the pressure and vacuum generator PGVA-2 from Festo.
© Festo SE & Co. KG
Sensapex - uMc pressure controllers
Higher throughput and accuracy: lab automation with uMc pressure controllers from Sensapex relying on piezo-based pressure regulators VEAB from Festo.
© Festo SE & Co. KG
2024/05/06
|
ワールドワイド
Extremely high sample throughput rates
If there’s one thing the corona pandemic has taught us, it is that laboratories place tremendous ...
プレスリリースを閲覧する
If there’s one thing the corona pandemic has taught us, it is that laboratories place tremendous importance on high sample throughput rates. Even with highly qualified laboratory personnel, this demand can no longer be met. There’s no getting round the automation of laboratory processes. That’s why MolGen in the Netherlands developed PurePrep TTR, which can prepare 320 patient samples per hour for molecular downstream processing. And ...
© Festo SE & Co. KG
DHOE pipetting head
An open pipetting system with pipetting head DHOE for simple liquid transport makes it possible to configure the most important pipetting functions based on requirements, and to expand them flexibly – the system is also compatible with the largest...