© Festo SE & Co. KG 2024/02/15 | Global Moving loads at the tip of two fingers Ergonomics improves efficiency thanks to a servo-pneumatic balancer that enables employees in assembly and ... Ler comunicados de imprensa Ergonomics improves efficiency thanks to a servo-pneumatic balancer that enables employees in assembly and logistics to lift and move loads effortlessly, using just two fingers. At the heart of the balancer is the powerful and reliable drive solution YHBP from Festo with automatic weight detection and safety Performance Level d – perfect for the automotive and packaging industries.
© Festo SE & Co. KG 2023/05/15 | Global Safe batteries for electric vehicles The success and reputation of electric vehicle manufacturers depend on the safe and flawless functioning of ... Ler comunicados de imprensa The success and reputation of electric vehicle manufacturers depend on the safe and flawless functioning of batteries. HAHN Automation Group has therefore developed a battery tester that carries out a complete test of the mobile energy storage units fully automatically. A 3-axis gantry for optical and leak tests, consisting of electric drives from Festo, takes centre stage.
© Festo SE & Co. KG 2023/03/16 | Global Optimising curing presses with AI Digitalisation and artificial intelligence (AI) are megatrends that can also offer great potential for savings ... Ler comunicados de imprensa Digitalisation and artificial intelligence (AI) are megatrends that can also offer great potential for savings in tyre production. Machine learning algorithms can be implemented in a decentralised manner, for example on the edge, i.e. on the actual module to be monitored. An example is Festo AX. This AI software uses these algorithms to detect anomalies on tyre building machines or in curing presses.
© Festo SE & Co. KG 2023/03/16 | Global Flexible interfaces in plant engineering Flexible, robust and offering high performance – the angle seat valve VZXA from Festo controls media ... Ler comunicados de imprensa Flexible, robust and offering high performance – the angle seat valve VZXA from Festo controls media flows quickly and reliably up to 230 °C. Its carefully thought-out product design and patented interface enable valve bodies and actuators to be freely combined, with a hot-swap function for quickly exchanging actuator or other spare parts.
2025/06/02 | Global Battery Show Europe 2025 Reliable, economical, sustainable: The circular battery life cycle – solutions from cell production ... Comunicados de imprensa (8) Imagens (30) Vídeos (0) Visualizar pasta de imprensa © Festo SE & Co. KG
2024/11/08 | Global SPS 2024 - The Automation ... The SPS from 12 – 14 November 2024 in Nuremberg is the industry highlight of the automation sector ... Comunicados de imprensa (7) Imagens (11) Vídeos (0) Visualizar pasta de imprensa © Festo SE & Co. KG
2024/06/24 | Global Battery Show Europe 2024 Reliable, economical, sustainable: The circular battery life cycle – solutions from cell production ... Comunicados de imprensa (4) Imagens (15) Vídeos (0) Visualizar pasta de imprensa © Festo SE & Co. KG
2023/05/22 | Global Battery Show Europe 2023 Reliable, economical, sustainable: The circular battery life cycle – solutions from cell production ... Comunicados de imprensa (6) Imagens (17) Vídeos (0) Visualizar pasta de imprensa © Festo SE & Co. KG