Cycle times reduced by 30 per cent
Compact design for 30% shorter cycle times and 50% less vibration – those are the most important characteristics of the cantilever axis with toothed belt ELCC-TB from Festo. The axis fits in seamlessly with Festo's concept of complete connectivity for its electric automation technology.
The high rigidity of the toothed belt cantilever axis cuts vibrations in half, whilst the low moving mass of the compact design reduces cycle times by almost a third. A stainless steel cover strip protects the internal recirculating ball bearing guide. Thanks to sealing air, the cantilever axis ELCC-TB is suitable for use in dusty environments or on machine tools. A clamping unit securely holds loads and acts as an emergency brake.
With a stroke of up to two metres, the cantilever axis is ideally installed vertically as a Z-axis, for example for palletising or erecting boxes. It can also be used horizontally or at any other installation angle if the axis has to be removed from the working space.
Complete connectivity
The cantilever axis ELCC-TC is an important part of Festo's philosophy of complete connectivity, i.e., the ability to connect a workpiece completely through to the cloud, from its mechanical connections and electrical interfaces to commissioning and controller programming. This simplifies the work of every machine builder and automation engineer when it comes to connecting the mechanical and electric technology as well as the control levels and their interfaces with the hardware and software.
费斯托 (Festo)是一家全球性的独立的家族企业,总部位于德国埃斯林根。自成立以来,Festo在工业自动化技术和技术教育方面制定标准,从而为环境、经济和社会的可持续发展做出贡献。公司为超过35个行业的30万家工厂和过程自动化客户提供气动和电驱动自动化技术解决方案,其中生命科学和实验室自动化业务受到越来越多的关注。Festo产品和服务遍布176个国家。2024年,费斯托在全球61个国家的250多个分支机构拥有约20600名员工,实现销售额34.5亿欧元。每年约8%的销售额用于研发。在这家学习型企业,1.5%的销售额用于基础和进一步培训。Festo 教学培训 (Didactic SE) 是全球领先的技术教育和培训供应商,为全球客户提供工业环境中全面的数字化和常规学习解决方案。