![](https://pressstorageadmin.blob.core.windows.net/prod/styles/content_header/storage-api-public/field/title32picture/TC_Altbau_von_oben_IMG_6869_13x18.jpg?sv=2017-11-09&sr=b&se=2025-07-17T00:42:33Z&sp=r&sig=HBmeBA7Z7Y0u1k8acl8a0Kl8zRAYriQUyVpG7KHdauk%3D&itok=-8-47HnH)
Compact, precise and reliable
More and more samples have to be analysed in ever shorter time. The laboratories have been under pressure not only since March. Reliable and fast automation solutions from Festo are the answer.
At present, the test results for Covid-19 are eagerly awaited, the waiting time for the common PCR tests is currently up to one week. However, sample results are sometimes erroneous, the reason? The processes in laboratories are still mainly carried out manually by humans. Doubts about the correctness of the results make people feel uncomfortable. This is where reliable and fast automation solutions are required.
Highlights at COMAPMED 2020
A highlight at this year's COMPAMED are ready-to-install solutions for in-vitro diagnostics in the field of Point of Care Testing (POCT). Compact analysis instruments make quick testing possible at the doctor’s office in order to identify the pathogen responsible for a cold or flu, as well as other bacterial or viral infections. In particular for this type of equipment, Festo offers ready-to-install automation solutions including customised engineering.
The compact rotary gripper module EHMD, which can grip and rotate sample vials, is unique on the market so far. It opens the smallest sample vials with a volume of up to 15 millilitres without any problems.
With the VYKA, a new media-separated solenoid valve for precise dispensing of liquids or control of liquid flows in manifold duct plates came onto the market. A current-controlled solenoid permits highly precise and reliable operation. Media separation ensures highest possible safety standards and chemical resistance. For higher flow rates the VYKB is used.
Components and subsystems for laboratory processes and medical devices
In addition to standard components, the LifeTech division develops separate components with new technologies that are designed specifically for laboratory processes and medical devices in Boston, a major hotspot of the life science market. When developing customised automation solutions for its customers, Festo follows the approach of working out engineering concepts together with the customer from the earliest planning phase onwards.
Product range for laboratory automation
Festo develops intelligent, tested subsystems for the automation of liquid media and sample handling applications.
The focus is on:
- Feeding and identification of test tubes
- Opening and closing of test tubes
- Feeding and aspiration of liquid media and solids
The applications involve the use of both electric and pneumatic actuators with motors, controllers, sample & liquid handling systems as well as grippers, sensors and camera systems.
Product range for medical technology
In the field of medical technology, Festo develops products and subsystems for medical devices.
The focus is on the efficient regulation and control of medical gases such as:
- Flow control with compact valves for ventilation and anaesthesia devices
- Pneumatic integration solutions for surgical devices
- Regulation of fluids in dental stations
费斯托 (Festo)是一家全球性的独立的家族企业,总部位于德国埃斯林根。自成立以来,Festo在工业自动化技术和技术教育方面制定标准,从而为环境、经济和社会的可持续发展做出贡献。公司为超过35个行业的30万家工厂和过程自动化客户提供气动和电驱动自动化技术解决方案,其中生命科学和实验室自动化业务受到越来越多的关注。Festo产品和服务遍布176个国家。2023年,费斯托在全球61个国家的250多个分支机构拥有约20600名员工,实现销售额36.5亿欧元。每年约7%的销售额用于研发。在这家学习型企业,1.5%的销售额用于基础和进一步培训。Festo 教学培训 (Didactic SE) 是全球领先的技术教育和培训供应商,为全球客户提供工业环境中全面的数字化和常规学习解决方案。