![](https://pressstorageadmin.blob.core.windows.net/prod/styles/content_header/storage-api-public/field/web_images/Control32cabinet32solutions.jpg?sv=2017-11-09&sr=b&se=2025-08-26T13:07:11Z&sp=r&sig=ix9JgxRq2Pgpc7zGPlj8y7gNtQMuUQyeJ9%2BNKMRp0OY%3D&itok=mDoGbkUA)
Optimized for control cabinet installation
There is a growing trend towards ever smaller control cabinets, and control systems, remote I/Os and valve terminals from Festo are no exception. The modular control system CPX-E and the universal valve terminal VTUG are now combined into one solution package.
The package offered by Festo, consisting of the modular automation system CPX-E and the universal valve terminal VTUG, is more compact and cost-efficient than other control cabinet solutions.
Can be used universally
The modular control system CPX-E is an automated system for factory and process automation. It consists of individual function modules which enable a flexible, modular design: depending on the module combination, the system can be configured as a purely remote I/O system with bus module or as a control system with control unit. The CPX-E's distinguishing features are its rapid signal processing and its compact assembly.
The universal valve terminal VTUG has been specially designed for installation in control cabinets and to save space. Thanks to the new manifold rail variant, check valves and fixed flow restrictors, the valve terminal is a true all-rounder in control cabinets. The topic of "simple installation" is self-explanatory: the installation of the valve terminal in a control cabinet wall with the new manifold rails means that tubing within the control cabinet is unnecessary. The variant with a front outlet direction has a clearly visible LED indicator and inscription label holder, enabling direct access to the manual override function. The practical hot-swap function allows individual valves to be replaced quickly during operation without the valve terminals having to be depressurised, which could result in production downtime.
Festo is a global player and an independent family-owned company with headquarters in Esslingen am Neckar, Germany. Festo has set standards in industrial automation technology and technical education ever since its establishment, thereby making a contribution to sustainable development of the environment, the economy and society. The company supplies pneumatic and electrical automation technology to 300,000 customers of factory and process automation in over 35 industries. Digitalization, AI and the LifeTech sector with medical technology and laboratory automation are becoming increasingly important. The products and services are available in 176 countries. With about 20,600 employees in over 250 branch offices in around 60 countries worldwide, Festo achieved a turnover of around €3.65 billion in 2023. Each year around 7% of this turnover is invested in research and development. In this learning company, 1.5 % of turnover is invested in basic and further training. Festo Didactic SE is a leading provider of technical education and training and offers its customers worldwide comprehensive digital and physical learning solutions in the industrial environment.