Optimized for control cabinet installation
There is a growing trend towards ever smaller control cabinets, and control systems, remote I/Os and valve terminals from Festo are no exception. The modular control system CPX-E and the universal valve terminal VTUG are now combined into one solution package.
The package offered by Festo, consisting of the modular automation system CPX-E and the universal valve terminal VTUG, is more compact and cost-efficient than other control cabinet solutions.
Can be used universally
The modular control system CPX-E is an automated system for factory and process automation. It consists of individual function modules which enable a flexible, modular design: depending on the module combination, the system can be configured as a purely remote I/O system with bus module or as a control system with control unit. The CPX-E's distinguishing features are its rapid signal processing and its compact assembly.
The universal valve terminal VTUG has been specially designed for installation in control cabinets and to save space. Thanks to the new manifold rail variant, check valves and fixed flow restrictors, the valve terminal is a true all-rounder in control cabinets. The topic of "simple installation" is self-explanatory: the installation of the valve terminal in a control cabinet wall with the new manifold rails means that tubing within the control cabinet is unnecessary. The variant with a front outlet direction has a clearly visible LED indicator and inscription label holder, enabling direct access to the manual override function. The practical hot-swap function allows individual valves to be replaced quickly during operation without the valve terminals having to be depressurised, which could result in production downtime.
费斯托 (Festo)是一家全球性的独立的家族企业,总部位于德国埃斯林根。自成立以来,Festo在工业自动化技术和技术教育方面制定标准,从而为环境、经济和社会的可持续发展做出贡献。公司为超过35个行业的30万家工厂和过程自动化客户提供气动和电驱动自动化技术解决方案,其中生命科学和实验室自动化业务受到越来越多的关注。Festo产品和服务遍布176个国家。2023年,费斯托在全球61个国家的250多个分支机构拥有约20600名员工,实现销售额36.5亿欧元。每年约7%的销售额用于研发。在这家学习型企业,1.5%的销售额用于基础和进一步培训。Festo 教学培训 (Didactic SE) 是全球领先的技术教育和培训供应商,为全球客户提供工业环境中全面的数字化和常规学习解决方案。