To mark the company's 100th anniversary, the automation specialist Festo has designed an extraordinary machine that will be presented for the first time at the Hannover Messe 2025. Based on the principle of a Rube Goldberg machine, it does not manufacture a specific product but tells the story of motion in automation technology that has significantly influenced the family-owned company. Lire le communiqué de presse Image Festo SE & Co. KG 2025/02/18 | Globale The Festo Incredible Machine celebrates its ... To mark the company's 100th anniversary, the automation specialist Festo has designed an ... Lire le communiqué de presse
Creating added value for customers through innovation has been the driving force behind the family-owned company from the very beginning and remains the key to Festo's success today. With its constant determination to make people's work easier and thus increase efficiency, Festo has shaped an entire era of industrial production. Today, the company is a global player and a front runner in automation technology, as well as a world leader in technical education and training. Festo's anniversary is being celebrated with employees, customers, and... Lire le communiqué de presse Image Festo SE & Co. KG 2025/01/17 | Globale Belgique Irlande Pays-Bas Grande-Bretagne Festo Celebrates its Centenary – 100 Years in ... Creating added value for customers through innovation has been the driving force behind the family ... Lire le communiqué de presse
Users today face the challenge of having to integrate different topics such as control and motion, AI, data integration and evaluation, predictive maintenance and much more into their applications at the same time, with short development cycles and ever new requirements. Festo AX Controls presents an automation portfolio that takes these requirements into account. The motto "from the workpiece to the cloud" is taken further here, and Festo AX Controls combines many software modules such as operating system, motion, visualization, high-level... Lire le communiqué de presse Image Festo SE & Co. KG 2024/11/07 | Globale More customer success through seamless data ... Users today face the challenge of having to integrate different topics such as control and motion ... Lire le communiqué de presse
On the shopfloor, machines not only deliver products, but also large amounts of data that are converted into information using artificial intelligence in such a way that they show humans specific optimization potential . Initial successes are visible: in hundreds of customer applications, solutions from the Festo AX Industrial Intelligence portfolio have reduced unplanned downtimes by up to 25 % and cut waste by 20 %. Lire le communiqué de presse Image Festo SE & Co. KG 2024/11/07 | Globale Added value from data reduces downtime and waste On the shopfloor, machines not only deliver products, but also large amounts of data that are ... Lire le communiqué de presse
With the personalized MyFesto dashboard at www.festo.com, Festo customers have a central overview of their current offers and service requests and can access all data on Festo products from their projects on MyFesto Projects. In future, Festo users will have it even easier: the System Configurator will give them a central point of access to the entire world of Festo engineering tools. Lire le communiqué de presse Image Festo SE & Co. KG 2024/11/07 | Globale Taking customers by the hand along the value ... With the personalized MyFesto dashboard at www.festo.com, Festo customers have a central overview of ... Lire le communiqué de presse
Innovative guide technology, high rigidity and guide load capacity for more load in the same installation space - these are the features of the new ELGD axis family from Festo. In addition, powerful drive elements offer high feed forces and accelerations for shorter cycle times, a long service life and less downtime. A stainless steel cover strip is friction-free on the outside and does not allow any particles to form there. This makes the drives in the axis family ideal for use in cleanrooms. Lire le communiqué de presse Image Festo SE & Co. KG 2024/11/07 | Globale Precise and dynamic Innovative guide technology, high rigidity and guide load capacity for more load in the same ... Lire le communiqué de presse
The new, optimized EMMB-ST and EMMT-ST stepper motor family in conjunction with the CMMT-ST-MP servo drive controller offers users a coordinated servo system at an attractive price. Lire le communiqué de presse Image Festo SE & Co. KG 2024/11/07 | Globale Attractive servo system in sight The new, optimized EMMB-ST and EMMT-ST stepper motor family in conjunction with the CMMT-ST-MP servo ... Lire le communiqué de presse
The powerful, compact and versatile HEPP electric gripper is suitable for a wide range of workpieces in electrical systems or applications without compressed air. It is optimized for electronics and small parts production, laboratory automation and special machine construction. Lire le communiqué de presse Image Festo SE & Co. KG 2024/11/07 | Global Powerful, compact and precise The powerful, compact and versatile HEPP electric gripper is suitable for a wide range of workpieces ... Lire le communiqué de presse
Fresh on the market, the Festo AX Controls automation portfolio is showing its open side: voraus robotik, an innovative software company from Hanover, is integrating its automation software into Festo AX Controls. With the software voraus.core, manufacturers, integrators and end users can easily create and execute solutions for a wide range of applications and optimize and monitor their entire automation. Lire le communiqué de presse Image Festo SE & Co. KG 2024/11/07 | Globale Festo AX Controls automation portfolio in use Fresh on the market, the Festo AX Controls automation portfolio is showing its open side: voraus ... Lire le communiqué de presse
Generating energy sustainably is one of the great challenges of our time - and green hydrogen is a building block of the solution. Hydrogen will play a key role in the future energy landscape and in the decarbonization of energy-intensive industries. Festo offers comprehensive automation solutions along the entire hydrogen value chain - on show at Hydrogen Expo in Hamburg from October 21 to 23, 2025 (hall B6, booth 6J40). Lire le communiqué de presse Image Festo SE & Co. KG 2024/10/23 | Globale Automation for green hydrogen Generating energy sustainably is one of the great challenges of our time - and green hydrogen is a ... Lire le communiqué de presse
Wherever inert gases need to be precisely controlled, the mass flow controller VEFC from Festo is the right choice. Thanks to piezo technology, it is compact and flexible, and offers an excellent price/performance ratio. It is especially suitable for use in electronics manufacturing, food production, and anywhere in machine building where shielding gas is required. Lire le communiqué de presse Image Festo SE & Co. KG 2024/09/12 | Globale Precise control of inert gases Wherever inert gases need to be precisely controlled, the mass flow controller VEFC from Festo is ... Lire le communiqué de presse
The Olympic Games in Paris are over – now another French metropolis is taking center stage: Lyon will host the 47th WorldSkills from September 10 to 15, 2024. The WorldSkills Championships will bring together more than 1,500 young people from over 65 countries and regions to compete in 62 competitions. Lire le communiqué de presse Image Festo SE & Co. KG 2024/09/02 | Globale After the Olympics in Paris, now the WorldSkills ... The Olympic Games in Paris are over – now another French metropolis is taking center stage: Lyon ... Lire le communiqué de presse
Festo is expanding its portfolio to include multilayer manifolds made of plastic (bonded manifolds) in order to be able to offer manufacturers of medical and laboratory equipment solutions from a single source. To this end, Festo is taking over the production systems and processes for manufacturing these complex plastic manifolds from Carville, a leading company in this field. Lire le communiqué de presse Image Festo SE & Co. KG 2024/06/06 | Global Festo Expands its Portfolio with Multilayer ... Festo is expanding its portfolio to include multilayer manifolds made of plastic (bonded manifolds) ... Lire le communiqué de presse
After years of strong growth, 2023 was a year of consolidation. Turnover was just below the previous year’s level (- 4.3% to around 3.65 billion euros). Festo continued to invest heavily in research and development and the expansion of regional market supply. The company sees good opportunities for growth again in the medium term. The automation of future markets, but also the qualification of the specialists required for this, offers Festo great potential for sustainable growth in the Automation and Didactic business. This includes segments... Lire le communiqué de presse Image Festo SE & Co. KG 2024/04/22 | Globale Festo sees good Growth Prospects After years of strong growth, 2023 was a year of consolidation. Turnover was just below the previous ... Lire le communiqué de presse
For more than 15 years, the Bionic Learning Network has been focusing on the fascination of flying. In addition to the technical decoding of bird flight, the team has researched and technologically implemented numerous other flying objects and their natural principles. With the BionicBee, the Bionic Learning Network has now for the first time developed a flying object that can fly in large numbers and completely autonomously in a swarm. The BionicBee will present its first flight show at the Hannover Messe 2024. Lire le communiqué de presse Image Festo SE & Co. KG 2024/04/21 | Globale Belgique Irlande Pays-Bas Grande-Bretagne Autonomous Flying in a Swarm For more than 15 years, the Bionic Learning Network has been focusing on the fascination of flying ... Lire le communiqué de presse
Superconductor technology enables the contactless movement and handling of objects – ideal for high-tech industries such as laboratory automation or biotechnology. At the Hannover Messe, Festo presents a concept for the fully automated filling and weighing of freeze-dry containers in cleanrooms. Thanks to SupraMotion levitation modules and products from the Festo automation portfolio for laboratory applications, the highest standards of cleaning and cleanliness can be met. Lire le communiqué de presse Image Festo SE & Co. KG 2024/04/19 | Globale Superconductor technology: Contactless working in ... Superconductor technology enables the contactless movement and handling of objects – ideal for high ... Lire le communiqué de presse