![](https://pressstorageadmin.blob.core.windows.net/prod/styles/content_header/storage-api-public/field/web_images/Gesamtanlage32VTEM32und32MCS.jpg?sv=2017-11-09&sr=b&se=2025-07-16T09:16:46Z&sp=r&sig=Qu3Me%2BdqI5GvGDUAgCzgNRfEbIuBxRYjvEpfub4Y2NU%3D&itok=3D72ODzG)
Format change at the push of a button
Fast and straightforward format changes on just one machine are at the top of the wish list of many packaging machine manufacturers and their customers. Innovations from Festo make these wishes come true. Enter the brand new Festo Motion Terminal and the Multi-Carrier-System® MCS.
The ability to automate the production or packaging of custom products right down to batches of 1 is a USP that will really set manufacturers of packaging machines apart from the competition. This is exactly what can be achieved with the Multi-Carrier-System® MCS and the Festo Motion Terminal.
Multi-Carrier-System®
The flexible modular transport system can be adapted to different formats via software at the push of a button. Different box sizes and the matching number of products are set directly in the Multi-Carrier-System® MCS using the freely positionable carriers. The products can be individually transported, grouped and synchronously packaged on the carriers.
The Multi-Carrier-System® is flexible to install and operate. It is easy to integrate into existing logistics thanks to the infeed and outfeed of carriers without additional transfer points. Acceleration, speed, grouping and synchronous motion can be freely defined, even in the closed recirculating system of the carriers. The modular MCS® is used only where it is needed by the process – within a station or in parallel with the flow process. Return transport of the recirculating carriers is ensured by an inexpensive servo-controlled belt drive.
Digital pneumatics
With the Festo Motion Terminal, pneumatic functions can be controlled via apps for the first time, without having to change or modify the hardware. From simple directional control valve functions to complex motion tasks, applications can be easily standardised.
The brand new Festo Motion Terminal VTEM catapults pneumatics into the age of Industry 4.0 ‒ with apps that can replace more than 50 individual components. All this is made possible by the latest developments in piezo technology and software. Thanks to the fast activation of new functions via motion app licences, machine developers can create a basic machine type and then select the relevant apps to equip it with different functions and features as requested by the customer. It doesn’t get much more flexible than that!
费斯托 (Festo)是一家全球性的独立的家族企业,总部位于德国埃斯林根。自成立以来,Festo在工业自动化技术和技术教育方面制定标准,从而为环境、经济和社会的可持续发展做出贡献。公司为超过35个行业的30万家工厂和过程自动化客户提供气动和电驱动自动化技术解决方案,其中生命科学和实验室自动化业务受到越来越多的关注。Festo产品和服务遍布176个国家。2023年,费斯托在全球61个国家的250多个分支机构拥有约20600名员工,实现销售额36.5亿欧元。每年约7%的销售额用于研发。在这家学习型企业,1.5%的销售额用于基础和进一步培训。Festo 教学培训 (Didactic SE) 是全球领先的技术教育和培训供应商,为全球客户提供工业环境中全面的数字化和常规学习解决方案。