Precise and robust
The essence of any mechanical switching device is an accurate response. That is exactly why it is designed to respond with precision. And why it can be installed, without backlash, in just a few steps. The manually and mechanically actuated valves from the VHEF and VMEF series from Festo follow precisely these mechanical principles.
Given that the conditions in the field are sometimes quite harsh, for example with sawdust in furniture production, or even in agricultural automation, a manual or mechanical valve must be able to withstand stresses. The manual and mechanically actuated valve series VMEF and VHEF work reliably even in these types of situations. The valves ensure accurate processes and represent extremely good value for money.
Whether the mechanism is triggered by a workpiece, a component or a person, manual or mechanical valves are the most direct way to control a process. They don't need any energy conversion, additional reaction times or long cables. The actuated plunger simply switches the valve and triggers the next step in the process.
Both valves are part of the Festo core product range and are therefore always available worldwide, no matter where in the world a machine or system is installed.
费斯托 (Festo)是一家全球性的独立的家族企业,总部位于德国埃斯林根。自成立以来,Festo在工业自动化技术和技术教育方面制定标准,从而为环境、经济和社会的可持续发展做出贡献。公司为超过35个行业的30万家工厂和过程自动化客户提供气动和电驱动自动化技术解决方案,其中生命科学和实验室自动化业务受到越来越多的关注。Festo产品和服务遍布176个国家。2024年,费斯托在全球61个国家的250多个分支机构拥有约20600名员工,实现销售额34.5亿欧元。每年约8%的销售额用于研发。在这家学习型企业,1.5%的销售额用于基础和进一步培训。Festo 教学培训 (Didactic SE) 是全球领先的技术教育和培训供应商,为全球客户提供工业环境中全面的数字化和常规学习解决方案。