2024/11/08
ID: 4885

Taking customers by the hand along the value creation process

Using Festo engineering tools online throughout the entire value chain

With the personalized MyFesto dashboard at www.festo.com, Festo customers have a central overview of their current offers and service requests and can access all data on Festo products from their projects on MyFesto Projects. In future, Festo users will have it even easier: the System Configurator will give them a central point of access to the entire world of Festo engineering tools.

The System Configurator opens up the entire tool landscape of the design phase: customers can use it to design, select, dimension and configure their individual automation systems as a complete machine topology. Users can also configure specific components or entire load cases - from the PLC, drive controllers and remote I/Os in the AP network through to IO-Link devices. This enables customized automation solutions that are precisely tailored to the respective requirements.

 

Seamless collaboration

The System Configurator enables the storage and management of projects, parts lists and design data and integrates seamlessly into MyFesto Projects. This allows different functions in the customer's company to work together on the same project, for example by giving development engineers and purchasers access to the same data during the ordering process.

 

But that's not all: consistent data management via Projects allows design data to be imported directly into the Festo Automation Suite for efficient commissioning of the devices. This consistency offers several advantages: it facilitates the transition from planning to implementation, significantly reduces the time required for commissioning and at the same time reduces the susceptibility to errors.

 

In this way, Festo literally takes customers by the hand along the entire value creation process – from planning, development and procurement through to commissioning and maintenance. This makes the implementation of projects considerably faster, simpler and more efficient.

费斯托 (Festo)是一家全球性的独立的家族企业,总部位于德国埃斯林根。自成立以来,Festo在工业自动化技术和技术教育方面制定标准,从而为环境、经济和社会的可持续发展做出贡献。公司为超过35个行业的30万家工厂和过程自动化客户提供气动和电驱动自动化技术解决方案,其中生命科学和实验室自动化业务受到越来越多的关注。Festo产品和服务遍布176个国家。2024年,费斯托在全球61个国家的250多个分支机构拥有约20600名员工,实现销售额34.5亿欧元。每年约8%的销售额用于研发。在这家学习型企业,1.5%的销售额用于基础和进一步培训。Festo 教学培训 (Didactic SE) 是全球领先的技术教育和培训供应商,为全球客户提供工业环境中全面的数字化和常规学习解决方案。

My Festo
© Festo SE & Co. KG
My Festo
An example of the engineering tools: Consistent data management via Projects allows design data to be imported directly into the Festo Automation Suite for efficient commissioning of the devices.

全球联络人

分享新闻稿