Festo 现在为其用户提供了更多便利:经典阀岛 CPV、MPA-L/S 和 VTUG 的成熟优势和所有实用功能现在都可以在多功能 VTUX 阀岛中找到。此外,AP-I 和 AP-A 通信系统为数字化生产提供了理想平台。这为电气和气动自动化提供了灵活性、开放式架构和无缝集成。 阅读新闻稿 图像 Festo SE & Co. KG 2026/04/19 | 全球 多种功能集于一身 Festo 现在为其用户提供了更多便利:经典阀岛 CPV、MPA-L/S 和 VTUG 的成熟优势和所有实用功能现在都可以在多功能 VTUX 阀岛中找到。此外,AP-I 和 AP-A ... 阅读新闻稿
Controlled Pneumatics is the revolutionary compressed air technology from Festo that is opening up new perspectives for pneumatics. Thanks to this technology, the pressure control of the compact proportional valve terminal VTEP is extremely sensitive, down to less than 1 mbar. This is perfect for applications such as wafer polishing or patch clamping in life science. In addition, Controlled Pneumatics uses high-precision piezo valves to reduce compressed air consumption by up to 50%. 阅读新闻稿 图像 Festo SE & Co. KG 2024/02/05 | Global Pneumatics Makes a Technological Leap with Piezo Controlled Pneumatics is the revolutionary compressed air technology from Festo that is opening up ... 阅读新闻稿
Festo is now making it even easier for its users: the functions of the classic valve terminals CPV, MPA-L/S and VTUG are now available under the umbrella of the convertible valve terminal VTUX. In addition, the AP-I and AP-A communication system creates the ideal platform for digitalized production. This brings flexibility and openness - true to the motto "Open Architecture". 阅读新闻稿 图像 Festo SE & Co. KG 2023/11/11 | Global Italy Many functions safe under the roof of VTUX Festo is now making it even easier for its users: the functions of the classic valve terminals CPV ... 阅读新闻稿
Dosing, aspirating and controlling extremely small quantities of aggressive liquids and gases is not a problem with the media-separated solenoid valve VYKA from Festo. This compact powerhouse has a width of only 7 mm and can dose and aspirate the extremely small amounts of liquid very precisely. It also meets the strict requirements for leak-tightness for gas applications. 阅读新闻稿 图像 Festo SE & Co. KG 2023/11/08 | 全球 Compact and leak-tight powerhouse Dosing, aspirating and controlling extremely small quantities of aggressive liquids and gases is not ... 阅读新闻稿
2026/04/24 | 全球 Interpack 2026 7. 至 2026 年 5 月 13 日,杜塞尔多夫展览中心 新闻稿 (7) 图像 (16) 查看新闻稿资料 图像 Festo SE & Co. KG
2023/11/13 | Global Productronica 2023 World's leading trade fair for electronics development and production where Festo shows latest innovations and solutions ... 新闻稿 (7) 图像 (22) 查看新闻稿资料 图像 Festo SE & Co. KG